<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックFlash Programming fails</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Flash-Programming-fails/m-p/491873#M12605</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using CodeWarrior 10.6.4 with a P&amp;amp;E USB-ML-UNIVERSAL cable to connect to a Kinetis K60DN512VLL10.&amp;nbsp; Flash programming and debugging fail.&amp;nbsp; I have captured a diagnostic zip file.&amp;nbsp; I was using this on a different computer just fine, but I upgraded my computer and now the setup doesn't work.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338650"&gt;201601140924_DiagnosticInfo.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jan 2016 17:03:07 GMT</pubDate>
    <dc:creator>carrieowen</dc:creator>
    <dc:date>2016-01-14T17:03:07Z</dc:date>
    <item>
      <title>Flash Programming fails</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Flash-Programming-fails/m-p/491873#M12605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using CodeWarrior 10.6.4 with a P&amp;amp;E USB-ML-UNIVERSAL cable to connect to a Kinetis K60DN512VLL10.&amp;nbsp; Flash programming and debugging fail.&amp;nbsp; I have captured a diagnostic zip file.&amp;nbsp; I was using this on a different computer just fine, but I upgraded my computer and now the setup doesn't work.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338650"&gt;201601140924_DiagnosticInfo.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jan 2016 17:03:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Flash-Programming-fails/m-p/491873#M12605</guid>
      <dc:creator>carrieowen</dc:creator>
      <dc:date>2016-01-14T17:03:07Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Programming fails</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Flash-Programming-fails/m-p/491874#M12606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carrie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is my configuration:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Win 7 64 bit&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CW for MCU V10.6.4 + Updates 5 &amp;amp; 6&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; TWR-K60D100M (Based on K60DN512)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Multilink Universal Rev B&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With this configuration I've created an example with the project Wizard.&lt;/P&gt;&lt;P&gt;After to have build the project I can launch the debug session for Ram and Flash targets without problem.&lt;/P&gt;&lt;P&gt;Using the Flash file to Target , it's working fine too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you try to create a sample project with the project Wizard ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;NXP Technical Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 15:31:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Flash-Programming-fails/m-p/491874#M12606</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2016-01-15T15:31:41Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Programming fails</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Flash-Programming-fails/m-p/491875#M12607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have created a sample project but get the same errors when programming or debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Carrie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 15:50:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Flash-Programming-fails/m-p/491875#M12607</guid>
      <dc:creator>carrieowen</dc:creator>
      <dc:date>2016-01-15T15:50:05Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Programming fails</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Flash-Programming-fails/m-p/491876#M12608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If a sample project is not working, the problem could be linked to the Multilink or to the Board.&lt;/P&gt;&lt;P&gt;Does the 2 lights (blue and orange) on Multilink are lighted ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To simplify I can say the blue is for the connection between PC and Multilink and orange for connection between the multilink and board.&lt;/P&gt;&lt;P&gt;Under Windows Device Manager the Mulilink 2.0 should be displayed&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33688i33FB7F6B98D8BE77/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Multilink is a P&amp;amp;E interface.&lt;/P&gt;&lt;P&gt;There are some FAQs on P&amp;amp;E web site.&lt;/P&gt;&lt;P&gt;Please have a look to:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/faqs/faq_view.cfm?id=211" title="http://www.pemicro.com/faqs/faq_view.cfm?id=211"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; P&amp;amp;E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools, debug probes, and …&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.pemicro.com/faqs/faq_view.cfm?id=29" title="http://www.pemicro.com/faqs/faq_view.cfm?id=29"&gt;P&amp;amp;E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools, debug probes, and …&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;NXP Technical Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 16:40:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Flash-Programming-fails/m-p/491876#M12608</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2016-01-15T16:40:01Z</dc:date>
    </item>
  </channel>
</rss>