<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB BDM driver for S12 suitable for Windows 10 64bits in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/USB-BDM-driver-for-S12-suitable-for-Windows-10-64bits/m-p/482251#M12484</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I bought a KIT33812ECUEVME Evaluation Board.&lt;/P&gt;&lt;P&gt;This kit contains a 'USB BDM Tool' (KITTBDMLEVME).&lt;/P&gt;&lt;P&gt;I tried to install several drivers on my PC (Windows 10) but when I plug it, it is still unrecognized.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Kit contain a CD with Codewarrior 5.0 which cannot be installed (not OK on Windows 10 64 bits ?). So I installed Codewarrior 5.2 which seems to be running correctly. But, as I said above, I cannot connect to my hardware due to USB driver malfunction.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there other version of Codewarrior and USB/BDM driver for MC9S12P128 debugging suitable for Windows 10 64bits ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Feb 2016 16:24:57 GMT</pubDate>
    <dc:creator>sebaboard</dc:creator>
    <dc:date>2016-02-23T16:24:57Z</dc:date>
    <item>
      <title>USB BDM driver for S12 suitable for Windows 10 64bits</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/USB-BDM-driver-for-S12-suitable-for-Windows-10-64bits/m-p/482251#M12484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I bought a KIT33812ECUEVME Evaluation Board.&lt;/P&gt;&lt;P&gt;This kit contains a 'USB BDM Tool' (KITTBDMLEVME).&lt;/P&gt;&lt;P&gt;I tried to install several drivers on my PC (Windows 10) but when I plug it, it is still unrecognized.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Kit contain a CD with Codewarrior 5.0 which cannot be installed (not OK on Windows 10 64 bits ?). So I installed Codewarrior 5.2 which seems to be running correctly. But, as I said above, I cannot connect to my hardware due to USB driver malfunction.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there other version of Codewarrior and USB/BDM driver for MC9S12P128 debugging suitable for Windows 10 64bits ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2016 16:24:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/USB-BDM-driver-for-S12-suitable-for-Windows-10-64bits/m-p/482251#M12484</guid>
      <dc:creator>sebaboard</dc:creator>
      <dc:date>2016-02-23T16:24:57Z</dc:date>
    </item>
    <item>
      <title>Re: USB BDM driver for S12 suitable for Windows 10 64bits</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/USB-BDM-driver-for-S12-suitable-for-Windows-10-64bits/m-p/482252#M12485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Riche,&lt;/P&gt;&lt;P&gt;according to KIT33812ECUEVME user guide, "Initial kits may include the &lt;STRONG&gt;P&amp;amp;E Multilink&lt;/STRONG&gt; as the USB to BDM Tool. Normal production kits will make use of the &lt;STRONG&gt;TBDML&lt;/STRONG&gt;. It is important to know which tool you are using so that the proper connection is selected when using CodeWarrior."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;officially, CW5.2 can support Microsoft Windows 10 32- and 64-bit, if you use &lt;STRONG&gt;P&amp;amp;E Multilink &lt;/STRONG&gt;interface, it can work for 64bit win10 well. if use &lt;STRONG&gt;TBDML, &lt;/STRONG&gt;it doesn't support TBDML Connection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so please make sure you use &lt;STRONG&gt;P&amp;amp;E Multilink &lt;/STRONG&gt;interface.&lt;/P&gt;&lt;P&gt;P&amp;amp;E also has "&lt;STRONG&gt;P&amp;amp;E Hardware Interface Drivers, Version 12 (Win XP/Vista/7/8/10)&lt;/STRONG&gt;" &lt;A href="http://www.pemicro.com/downloads/download_file.cfm?download_id=53" title="http://www.pemicro.com/downloads/download_file.cfm?download_id=53"&gt;http://www.pemicro.com/downloads/download_file.cfm?download_id=53&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/downloads/download_file.cfm?download_id=53" title="http://www.pemicro.com/downloads/download_file.cfm?download_id=53"&gt;http://www.pemicro.com/downloads/download_file.cfm?download_id=53&lt;/A&gt; &lt;/P&gt;&lt;P&gt;you can install it if necessary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can this help you?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Feb 2016 06:53:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/USB-BDM-driver-for-S12-suitable-for-Windows-10-64bits/m-p/482252#M12485</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-02-24T06:53:14Z</dc:date>
    </item>
  </channel>
</rss>