<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Timer Interrupt doesn't occur</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timer-Interrupt-doesn-t-occur/m-p/480074#M12468</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexandros,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition to Alice comments.&lt;/P&gt;&lt;P&gt;You're using CW for MCU V6.X which is a classic version.&lt;/P&gt;&lt;P&gt;Processor Expert is included and some examples too.&lt;/P&gt;&lt;P&gt;Please have a look to the folder:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; \CodeWarrior for Microcontrollers V6.3\ProcessorExpert\Projects\Test projects&lt;/P&gt;&lt;P&gt;You will find an example for each feature beans listed in the folder.&lt;/P&gt;&lt;P&gt;This example can be converted to the processor you're using.&lt;/P&gt;&lt;P&gt;To do that you just need to add a new processor and to select it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will help.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;NXP Technical Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Jan 2016 08:21:25 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2016-01-11T08:21:25Z</dc:date>
    <item>
      <title>Timer Interrupt doesn't occur</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timer-Interrupt-doesn-t-occur/m-p/480072#M12466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi! I am using codewarrior for device MC9RS08LA8RM(CFT) and I have set up via processor expert to generate an interrupt when timer overflows.&lt;/P&gt;&lt;P&gt;Here are settings and code&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fs21.postimg.org%2Fakegljq3b%2F1_10_2016a.jpg" rel="nofollow" target="_blank"&gt;http://s21.postimg.org/akegljq3b/1_10_2016a.jpg&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fs27.postimg.org%2Fop6cp5d7n%2F1_10_2016b.jpg" rel="nofollow" target="_blank"&gt;http://s27.postimg.org/op6cp5d7n/1_10_2016b.jpg&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fs10.postimg.org%2Fj783m8t4p%2F1_10_2016c.jpg" rel="nofollow" target="_blank"&gt;http://s10.postimg.org/j783m8t4p/1_10_2016c.jpg&lt;/A&gt; &lt;/P&gt;&lt;P&gt;It seems that there isn't any ISR at main.c file. When I debug no interrupt occurs to send program execution to ISR. but since ISR doesn't exist it stays at for loop. That's what it seems.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 10 Jan 2016 19:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timer-Interrupt-doesn-t-occur/m-p/480072#M12466</guid>
      <dc:creator>BlueTower</dc:creator>
      <dc:date>2016-01-10T19:05:40Z</dc:date>
    </item>
    <item>
      <title>Re: Timer Interrupt doesn't occur</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timer-Interrupt-doesn-t-occur/m-p/480073#M12467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Sorry , your pictures are so small that i can not see them clearly.&lt;/P&gt;&lt;P&gt;And what about the version of CW ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jan 2016 02:52:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timer-Interrupt-doesn-t-occur/m-p/480073#M12467</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-01-11T02:52:40Z</dc:date>
    </item>
    <item>
      <title>Re: Timer Interrupt doesn't occur</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timer-Interrupt-doesn-t-occur/m-p/480074#M12468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexandros,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition to Alice comments.&lt;/P&gt;&lt;P&gt;You're using CW for MCU V6.X which is a classic version.&lt;/P&gt;&lt;P&gt;Processor Expert is included and some examples too.&lt;/P&gt;&lt;P&gt;Please have a look to the folder:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; \CodeWarrior for Microcontrollers V6.3\ProcessorExpert\Projects\Test projects&lt;/P&gt;&lt;P&gt;You will find an example for each feature beans listed in the folder.&lt;/P&gt;&lt;P&gt;This example can be converted to the processor you're using.&lt;/P&gt;&lt;P&gt;To do that you just need to add a new processor and to select it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will help.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;NXP Technical Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jan 2016 08:21:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timer-Interrupt-doesn-t-occur/m-p/480074#M12468</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2016-01-11T08:21:25Z</dc:date>
    </item>
    <item>
      <title>Re: Timer Interrupt doesn't occur</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timer-Interrupt-doesn-t-occur/m-p/480075#M12469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok&amp;nbsp; see these images:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6736i1C00DCC45BD12D24/image-size/large?v=v2&amp;amp;px=999" title="1_10_2016a.jpg" alt="1_10_2016a.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6797iE28DE9CCB3A45B13/image-size/large?v=v2&amp;amp;px=999" title="1_10_2016b.jpg" alt="1_10_2016b.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6832i50EBF54D7CAB8D84/image-size/large?v=v2&amp;amp;px=999" title="1_10_2016c.jpg" alt="1_10_2016c.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where do I find header files for TimerInt project?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jan 2016 14:20:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timer-Interrupt-doesn-t-occur/m-p/480075#M12469</guid>
      <dc:creator>BlueTower</dc:creator>
      <dc:date>2016-01-11T14:20:36Z</dc:date>
    </item>
    <item>
      <title>Re: Timer Interrupt doesn't occur</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timer-Interrupt-doesn-t-occur/m-p/480076#M12470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexandros,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your project is using Device Initialization feature.&lt;/P&gt;&lt;P&gt;This feature is not generated code as Processor Expert but only intialization of the perhipheral which is defined in the MCUinit.c and .h files&lt;/P&gt;&lt;P&gt;Processor Expert includes some function to manage the peripheral.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some information extracted of help:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36037iFC5E434C6E9F2B32/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;To access this help, please click on Help Tab on Device Initialization Component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need more generated code, you need to select Processor Expert instead of Device Initialization.&lt;/P&gt;&lt;P&gt;Another option is to not use these features too.&lt;/P&gt;&lt;P&gt;There are examples in the folder \CodeWarrior for Microcontrollers V6.3\(CodeWarrior_Examples)\RS08\Assembly Examples\&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;NXP Technical Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 07:46:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Timer-Interrupt-doesn-t-occur/m-p/480076#M12470</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2016-01-13T07:46:27Z</dc:date>
    </item>
  </channel>
</rss>