<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 generate code for gpio and a/d</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/generate-code-for-gpio-and-a-d/m-p/467587#M12284</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am new to CodeWarrior and was informed there is a function which can generate code for interface with Pins.&amp;nbsp; I need to setup the A to D converter also some GPIO lines for input and output (not the same lines)?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I need help in how to use the application as well as what the application is to perform this function.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yours truly,&lt;/P&gt;&lt;P&gt;John Vogel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Dec 2015 12:28:37 GMT</pubDate>
    <dc:creator>haroldvogel</dc:creator>
    <dc:date>2015-12-08T12:28:37Z</dc:date>
    <item>
      <title>generate code for gpio and a/d</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/generate-code-for-gpio-and-a-d/m-p/467587#M12284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am new to CodeWarrior and was informed there is a function which can generate code for interface with Pins.&amp;nbsp; I need to setup the A to D converter also some GPIO lines for input and output (not the same lines)?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I need help in how to use the application as well as what the application is to perform this function.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yours truly,&lt;/P&gt;&lt;P&gt;John Vogel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 12:28:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/generate-code-for-gpio-and-a-d/m-p/467587#M12284</guid>
      <dc:creator>haroldvogel</dc:creator>
      <dc:date>2015-12-08T12:28:37Z</dc:date>
    </item>
    <item>
      <title>Re: generate code for gpio and a/d</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/generate-code-for-gpio-and-a-d/m-p/467588#M12285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Harold&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;User can use Processor Expert to easily configure a pin, or a peripheral module including ADC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When creating a new bareboard project in CodeWarrior, please enable the option of ‘Processor Expert’.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="PE.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59061i1FBF92DCB818657A/image-size/large?v=v2&amp;amp;px=999" role="button" title="PE.png" alt="PE.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For how to use Processor Expert, please refer to its help documents, usually it is:&lt;/P&gt;&lt;P&gt;C:\Freescale\CW MCU v10.6.4\MCU\Help\PDF\ProcessorExpertHelp.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For how to use each bean, please read the bean’s help pages. To open them, please place the mouse on the bean’s name in Components View, and right click the mouse and select Help. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Help.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59099i89D4124A84B39624/image-size/large?v=v2&amp;amp;px=999" role="button" title="Help.png" alt="Help.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Fiona Kuang&lt;/P&gt;&lt;P&gt;Technical Information &amp;amp; Commercial Support&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Dec 2015 03:46:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/generate-code-for-gpio-and-a-d/m-p/467588#M12285</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2015-12-10T03:46:23Z</dc:date>
    </item>
    <item>
      <title>Re: generate code for gpio and a/d</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/generate-code-for-gpio-and-a-d/m-p/467589#M12286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the information and help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Being new to code warrior this is great information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Dec 2015 11:40:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/generate-code-for-gpio-and-a-d/m-p/467589#M12286</guid>
      <dc:creator>haroldvogel</dc:creator>
      <dc:date>2015-12-10T11:40:52Z</dc:date>
    </item>
  </channel>
</rss>