<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Source Code is Missing on degugging in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Source-Code-is-Missing-on-degugging/m-p/467184#M12273</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hitoshi,&lt;/P&gt;&lt;P&gt;Which version Code Warrior do you used ? CW10.6 CW 10.5 or anything else ?&lt;/P&gt;&lt;P&gt;Which chip do you used ?&lt;/P&gt;&lt;P&gt;And have you test create one simple project ,then&amp;nbsp; build , debug ?&lt;/P&gt;&lt;P&gt;You said when debug it shows&amp;nbsp; "No Source available for XX". do you meaning &lt;/P&gt;&lt;P&gt;when build it have no error ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can take a screenshot about the error and your steps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Jun 2016 02:39:02 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2016-06-01T02:39:02Z</dc:date>
    <item>
      <title>Source Code is Missing on degugging</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Source-Code-is-Missing-on-degugging/m-p/467183#M12272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;My configuration with Code Warrior 10 has problem.&lt;/P&gt;&lt;P&gt;Before I knew it, My configuration is missing source code for a project. it alway say "No Source available for XX".&lt;/P&gt;&lt;P&gt;I can create break point on a source code, it looks work fine, Disassembly window show correct part,&amp;nbsp; valiables shows correct values, just source code does not show it.&lt;/P&gt;&lt;P&gt;I have confirmed debug configuration&amp;gt;source. there is default, it includes target project folder.&lt;/P&gt;&lt;P&gt;I have compared coworkers it handles same project. I cannot any defference with these settings but it works well, not same as mine.&lt;/P&gt;&lt;P&gt;I have also tried to uninstall / install Code Warrior, Create new workspace with new project. it meaning there are no .metadata or .setting. but still my configuration cannot find source files.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Would you like to give me any suggestion for me?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 00:21:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Source-Code-is-Missing-on-degugging/m-p/467183#M12272</guid>
      <dc:creator>hitoshihosaka</dc:creator>
      <dc:date>2016-06-01T00:21:31Z</dc:date>
    </item>
    <item>
      <title>Re: Source Code is Missing on degugging</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Source-Code-is-Missing-on-degugging/m-p/467184#M12273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hitoshi,&lt;/P&gt;&lt;P&gt;Which version Code Warrior do you used ? CW10.6 CW 10.5 or anything else ?&lt;/P&gt;&lt;P&gt;Which chip do you used ?&lt;/P&gt;&lt;P&gt;And have you test create one simple project ,then&amp;nbsp; build , debug ?&lt;/P&gt;&lt;P&gt;You said when debug it shows&amp;nbsp; "No Source available for XX". do you meaning &lt;/P&gt;&lt;P&gt;when build it have no error ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can take a screenshot about the error and your steps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 02:39:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Source-Code-is-Missing-on-degugging/m-p/467184#M12273</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-06-01T02:39:02Z</dc:date>
    </item>
  </channel>
</rss>