<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How can I generate position independent code for an MPC5607B (VLE code) with CodeWarrior V10.6.4? in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-can-I-generate-position-independent-code-for-an-MPC5607B-VLE/m-p/448912#M12056</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Stephan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't think there is any special compiler/linker setting to link the project executing with position independent code/data.&amp;nbsp; &lt;/P&gt;&lt;P&gt;I recommend to put bootloader image and the user application image into different sectors in the internal flash.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fiona Kuang&lt;/P&gt;&lt;P&gt;Technical Information &amp;amp; Commercial Support&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Nov 2015 05:15:24 GMT</pubDate>
    <dc:creator>TICS_Fiona</dc:creator>
    <dc:date>2015-11-03T05:15:24Z</dc:date>
    <item>
      <title>How can I generate position independent code for an MPC5607B (VLE code) with CodeWarrior V10.6.4?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-can-I-generate-position-independent-code-for-an-MPC5607B-VLE/m-p/448911#M12055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am currently working on a bootloader software for an MPC5607B which exclusively uses VLE code (virtual length encoding). My problem is that CodeWarrior V10.6.4 does not support code model "SDA based PIC/PID Addressing" for MPC5607B because it uses VLE code. Is there any other way that I can generate position independent code? Any help appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 31 Oct 2015 17:22:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-can-I-generate-position-independent-code-for-an-MPC5607B-VLE/m-p/448911#M12055</guid>
      <dc:creator>stephanmorgenst</dc:creator>
      <dc:date>2015-10-31T17:22:55Z</dc:date>
    </item>
    <item>
      <title>Re: How can I generate position independent code for an MPC5607B (VLE code) with CodeWarrior V10.6.4?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-can-I-generate-position-independent-code-for-an-MPC5607B-VLE/m-p/448912#M12056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Stephan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't think there is any special compiler/linker setting to link the project executing with position independent code/data.&amp;nbsp; &lt;/P&gt;&lt;P&gt;I recommend to put bootloader image and the user application image into different sectors in the internal flash.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fiona Kuang&lt;/P&gt;&lt;P&gt;Technical Information &amp;amp; Commercial Support&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Nov 2015 05:15:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-can-I-generate-position-independent-code-for-an-MPC5607B-VLE/m-p/448912#M12056</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2015-11-03T05:15:24Z</dc:date>
    </item>
  </channel>
</rss>