<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックerror in code-warrior stating:Vector allocated at absolute address , overlaps with sections placed in segment</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/error-in-code-warrior-stating-Vector-allocated-at-absolute/m-p/447731#M12031</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i am a new bee to the freescale family. i have installed code warrior and trying to run the code in simulator. it was all good and i was able to carry out debugging etc.&lt;/P&gt;&lt;P&gt;but when i tried copying the code from the example program i ended up getting this particular error.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Description Resource Path Location Type Vector allocated at absolute address 0xDFFE overlaps with sections placed in segment .absSeg0 201510081600 C/C++ Problem&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;please also look into this discission &lt;A _jive_internal="true" data-containerid="2016" data-containertype="14" data-objectid="62059" data-objecttype="1" href="https://community.nxp.com/thread/62059"&gt;L1119: Vector allocated at absolute address 0xFFFE overlaps with sections placed in segment .absSeg2&lt;/A&gt;&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;they specify a particular file called the PRM file te the above discussion can i know wat actually is this file and where it is located. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks in advance for your valuable time and support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Oct 2015 07:33:59 GMT</pubDate>
    <dc:creator>nishilraj</dc:creator>
    <dc:date>2015-10-09T07:33:59Z</dc:date>
    <item>
      <title>error in code-warrior stating:Vector allocated at absolute address , overlaps with sections placed in segment</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/error-in-code-warrior-stating-Vector-allocated-at-absolute/m-p/447731#M12031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i am a new bee to the freescale family. i have installed code warrior and trying to run the code in simulator. it was all good and i was able to carry out debugging etc.&lt;/P&gt;&lt;P&gt;but when i tried copying the code from the example program i ended up getting this particular error.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Description Resource Path Location Type Vector allocated at absolute address 0xDFFE overlaps with sections placed in segment .absSeg0 201510081600 C/C++ Problem&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;please also look into this discission &lt;A _jive_internal="true" data-containerid="2016" data-containertype="14" data-objectid="62059" data-objecttype="1" href="https://community.nxp.com/thread/62059"&gt;L1119: Vector allocated at absolute address 0xFFFE overlaps with sections placed in segment .absSeg2&lt;/A&gt;&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;they specify a particular file called the PRM file te the above discussion can i know wat actually is this file and where it is located. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks in advance for your valuable time and support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 07:33:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/error-in-code-warrior-stating-Vector-allocated-at-absolute/m-p/447731#M12031</guid>
      <dc:creator>nishilraj</dc:creator>
      <dc:date>2015-10-09T07:33:59Z</dc:date>
    </item>
    <item>
      <title>Re: error in code-warrior stating:Vector allocated at absolute address , overlaps with sections placed in segment</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/error-in-code-warrior-stating-Vector-allocated-at-absolute/m-p/447732#M12032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When an application is build 2 operations are done (this is true for all architectures):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - compile all source files and generate object files,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - merge all objects in 1 executable file (debug and Srecord files are generated) according to the linker parameter file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For HC08 and HC12 the linker parameter file is named prm file and uses prm as extension for instance "test.prm".&lt;/P&gt;&lt;P&gt;This file should be located under your project.&lt;/P&gt;&lt;P&gt;I recommend to perform a search with "*.prm".&lt;/P&gt;&lt;P&gt;In all case this file should be listed somewhere in your project too via the project IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you've a linker error L1119, it means the same address is used 2 times in your application.&lt;/P&gt;&lt;P&gt;Most of the time the default project includes vector table and all peripheral definitions.&lt;/P&gt;&lt;P&gt;If the objects are defined a second time, the linker generates this type of error.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Oct 2015 07:15:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/error-in-code-warrior-stating-Vector-allocated-at-absolute/m-p/447732#M12032</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-10-20T07:15:54Z</dc:date>
    </item>
  </channel>
</rss>