<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: remove file properties</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/remove-file-properties/m-p/430754#M11798</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you use CodeWarrior ? Which version ? And about which chip ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Nov 2015 03:15:33 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2015-11-23T03:15:33Z</dc:date>
    <item>
      <title>remove file properties</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/remove-file-properties/m-p/430753#M11797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How do I remove properties (such as optimization settings) set for a specific file so that it reverts back to using those for the folder or project ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 18:32:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/remove-file-properties/m-p/430753#M11797</guid>
      <dc:creator>asmith</dc:creator>
      <dc:date>2015-11-20T18:32:02Z</dc:date>
    </item>
    <item>
      <title>Re: remove file properties</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/remove-file-properties/m-p/430754#M11798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you use CodeWarrior ? Which version ? And about which chip ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Nov 2015 03:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/remove-file-properties/m-p/430754#M11798</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-11-23T03:15:33Z</dc:date>
    </item>
    <item>
      <title>Re: remove file properties</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/remove-file-properties/m-p/430755#M11799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The configuration can be linked to the project (all files included), folder or specific to a file.&lt;/P&gt;&lt;P&gt;If the properties is opened when the project is selected you will open the Project Properties.&lt;/P&gt;&lt;P&gt;If the properties is opened when a file is selected, you will open the file properties.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The File properties is applied on file only whereas the project properties is applied on all files included in the project.&lt;/P&gt;&lt;P&gt;If you open the file properties and click on "Restore Defaults" the options defined in the project properties will be applied.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you've a specific Folder properties (different to project) when "Restore Defaults" is applied on file the options defined in the project are used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will answer your question&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Nov 2015 14:45:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/remove-file-properties/m-p/430755#M11799</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-11-23T14:45:24Z</dc:date>
    </item>
  </channel>
</rss>