<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: printf() support in Processor Expert ConsoleIO in Codewarrior 10.6</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/printf-support-in-Processor-Expert-ConsoleIO-in-Codewarrior-10-6/m-p/428177#M11760</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just reproduced your problem, it is because the current clock setting can't set accurate 115200 baud rate. if i set baud rate as 9600, it can work. see attached video &lt;SPAN class="defaultSkin"&gt;&lt;SPAN class="jive-icon-med jive-icon-doctype-generic"&gt;&lt;/SPAN&gt;&lt;SPAN class="j-attachment-name-chop"&gt;baud rate 9600.mp4&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;or if you need 115200 baud rate anyway, we can trim&amp;nbsp; internal reference clock to 31.25. and set MCGOUT as 20M. it works for 115200 baud rate. see below screenshot. see attached video&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can it help you?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Aug 2015 10:19:47 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2015-08-25T10:19:47Z</dc:date>
    <item>
      <title>printf() support in Processor Expert ConsoleIO in Codewarrior 10.6</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/printf-support-in-Processor-Expert-ConsoleIO-in-Codewarrior-10-6/m-p/428176#M11759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;There is once a method that can debug Firmware program with printing message into CodeWarrior Console instead of output to h/w Uart&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;It’s helpful to debug communication procedure in slave mode, if the received data can be pushed into CodeWarrior Console&amp;nbsp; for view.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #1f497d;"&gt;URL: &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fmcuoneclipse.com%2F2013%2F02%2F07%2Ftutorial-printf-with-and-without-processor-expert%2F" rel="nofollow" target="_blank"&gt;http://mcuoneclipse.com/2013/02/07/tutorial-printf-with-and-without-processor-expert/&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Above is for CodeWarrior 10.3, but when use 10.6. Per checked, there is no valid ConsoleIO component in 10.6. pls see attached screen capture file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN style="color: #1f497d;"&gt; &lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Any idea on print message in Console for debug?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;BR/Roger&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2015 09:44:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/printf-support-in-Processor-Expert-ConsoleIO-in-Codewarrior-10-6/m-p/428176#M11759</guid>
      <dc:creator>Roger_Fan</dc:creator>
      <dc:date>2015-08-10T09:44:22Z</dc:date>
    </item>
    <item>
      <title>Re: printf() support in Processor Expert ConsoleIO in Codewarrior 10.6</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/printf-support-in-Processor-Expert-ConsoleIO-in-Codewarrior-10-6/m-p/428177#M11760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just reproduced your problem, it is because the current clock setting can't set accurate 115200 baud rate. if i set baud rate as 9600, it can work. see attached video &lt;SPAN class="defaultSkin"&gt;&lt;SPAN class="jive-icon-med jive-icon-doctype-generic"&gt;&lt;/SPAN&gt;&lt;SPAN class="j-attachment-name-chop"&gt;baud rate 9600.mp4&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;or if you need 115200 baud rate anyway, we can trim&amp;nbsp; internal reference clock to 31.25. and set MCGOUT as 20M. it works for 115200 baud rate. see below screenshot. see attached video&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can it help you?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Aug 2015 10:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/printf-support-in-Processor-Expert-ConsoleIO-in-Codewarrior-10-6/m-p/428177#M11760</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-08-25T10:19:47Z</dc:date>
    </item>
  </channel>
</rss>