<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Processor Expert - Add in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert-Add/m-p/417292#M11676</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am attempting to add a component to an existing project using the processor expert facility.&amp;nbsp; The component is an I2C component.&amp;nbsp; When I right click on the component in an attempt to add it to the existing project the "add to project" is greyed out. &lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What am I doing wrong or is this yet another issue with Code Warrior 10.6?&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have attached the project.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338844"&gt;project.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Sep 2015 16:55:18 GMT</pubDate>
    <dc:creator>ronaldpatton</dc:creator>
    <dc:date>2015-09-01T16:55:18Z</dc:date>
    <item>
      <title>Processor Expert - Add</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert-Add/m-p/417292#M11676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am attempting to add a component to an existing project using the processor expert facility.&amp;nbsp; The component is an I2C component.&amp;nbsp; When I right click on the component in an attempt to add it to the existing project the "add to project" is greyed out. &lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What am I doing wrong or is this yet another issue with Code Warrior 10.6?&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have attached the project.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338844"&gt;project.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Sep 2015 16:55:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert-Add/m-p/417292#M11676</guid>
      <dc:creator>ronaldpatton</dc:creator>
      <dc:date>2015-09-01T16:55:18Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert - Add</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert-Add/m-p/417293#M11677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ronald,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The project sent doesn't include Processor Expert.&lt;/P&gt;&lt;P&gt;I've created a project based on mc9s08qg8 with the wizard including Processor Expert.&lt;/P&gt;&lt;P&gt;I can add the InternalI2C bean without problem and build the project.&lt;/P&gt;&lt;P&gt;I'm using CW for MCU v10.6.4 +Patch 10.6.5 which is the last version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached you will find the example.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 09:54:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert-Add/m-p/417293#M11677</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-09-04T09:54:05Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert - Add</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert-Add/m-p/417294#M11678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OK, I have brought up the test project, but the chip is wrong.&amp;nbsp;&amp;nbsp; Your test project has MC9S08QG8CFK.&amp;nbsp; I need MC9S08QG8&lt;EM style="text-decoration: underline;"&gt;CPBE&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ron Patton&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 12:59:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert-Add/m-p/417294#M11678</guid>
      <dc:creator>ronaldpatton</dc:creator>
      <dc:date>2015-09-04T12:59:03Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert - Add</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert-Add/m-p/417295#M11679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ron,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can change the device in the project sent or ...&lt;/P&gt;&lt;P&gt;I've created a new project for QG8 and changed the device.&lt;/P&gt;&lt;P&gt;To do that, click on Components Library and select the processor family: HCS08 - QA/QD/QG - MC9S08QG8.&lt;/P&gt;&lt;P&gt;Now in the dialog you can select the MC9S08QG8CPB.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54784iCABCD99E42383C01/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Then I added the InternalI2C bean.&lt;/P&gt;&lt;P&gt;Attached the new project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 13:48:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert-Add/m-p/417295#M11679</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-09-04T13:48:39Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert - Add</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert-Add/m-p/417296#M11680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, thanks.&amp;nbsp; That worked.&amp;nbsp; Now I will determine if the existing project source code will compile and build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ron Patton&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 14:37:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert-Add/m-p/417296#M11680</guid>
      <dc:creator>ronaldpatton</dc:creator>
      <dc:date>2015-09-04T14:37:24Z</dc:date>
    </item>
  </channel>
</rss>