<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: How do I disable the &amp;quot;Always Erase and Program flash without asking&amp;quot; option in the Hardware Connection Advanced Programming Options?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-do-I-disable-the-quot-Always-Erase-and-Program-flash-without/m-p/413100#M11646</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matt,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Apologies for the delayed response, I have just received confirmation from P&amp;amp;E that there is no way to disable the "Always Erase and Program flash without asking" option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jul 2015 14:28:34 GMT</pubDate>
    <dc:creator>Carlos_Mendoza</dc:creator>
    <dc:date>2015-07-16T14:28:34Z</dc:date>
    <item>
      <title>How do I disable the "Always Erase and Program flash without asking" option in the Hardware Connection Advanced Programming Options?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-do-I-disable-the-quot-Always-Erase-and-Program-flash-without/m-p/413099#M11645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;this is a re-post of &lt;A _jive_internal="true" data-containerid="2028" data-containertype="14" data-objectid="337247" data-objecttype="1" href="https://community.nxp.com/thread/337247?commentID=498116#comment-498116"&gt;Re: How do I disable the "Always Erase and Program flash without asking" option in the Hardware Connection Advanced Prog…&lt;/A&gt; There is a separate issue around software breakpoints that is being addressed by our FAE; however, we would like to figure this out as it adds a lot of time when debugging...&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, in a CodeWarrior10.6 project, when we download our image to external RAM for debugging CodeWarrior always attempts to write to flash. This takes a long time to time-out and fail; we cannot disable this option. Help!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="32812_32812.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120367i393F25BB6FC727A3/image-size/large?v=v2&amp;amp;px=999" role="button" title="32812_32812.png" alt="32812_32812.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Advanced_Programming_Options.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/28021iAE402E5F6CE8F6FB/image-size/large?v=v2&amp;amp;px=999" role="button" title="Advanced_Programming_Options.png" alt="Advanced_Programming_Options.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2015 20:21:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-do-I-disable-the-quot-Always-Erase-and-Program-flash-without/m-p/413099#M11645</guid>
      <dc:creator>mjosborne</dc:creator>
      <dc:date>2015-05-29T20:21:51Z</dc:date>
    </item>
    <item>
      <title>Re: How do I disable the "Always Erase and Program flash without asking" option in the Hardware Connection Advanced Programming Options?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-do-I-disable-the-quot-Always-Erase-and-Program-flash-without/m-p/413100#M11646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matt,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Apologies for the delayed response, I have just received confirmation from P&amp;amp;E that there is no way to disable the "Always Erase and Program flash without asking" option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2015 14:28:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-do-I-disable-the-quot-Always-Erase-and-Program-flash-without/m-p/413100#M11646</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2015-07-16T14:28:34Z</dc:date>
    </item>
  </channel>
</rss>