<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックKL16Z256M4 Codewarrior setup &amp;quot;vague&amp;quot; error: Which name?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/KL16Z256M4-Codewarrior-setup-quot-vague-quot-error-Which-name/m-p/412161#M11640</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With Multylink programmer connected to Freescale MCU KL16Z256M4, an error is reported back&amp;nbsp; in Hardware Connection&amp;gt;&amp;gt;Advanced Programming Options:&amp;nbsp; "Device name could not be determined". &lt;/P&gt;&lt;P&gt;Which name? Is just the name it's missing? Never had seen this error!&lt;/P&gt;&lt;P&gt;Setup settings and MCU are ok since it work correctly on different machines. Any clue for this "vague" error.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;David Palma&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Sep 2015 16:45:20 GMT</pubDate>
    <dc:creator>djmp</dc:creator>
    <dc:date>2015-09-25T16:45:20Z</dc:date>
    <item>
      <title>KL16Z256M4 Codewarrior setup "vague" error: Which name?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/KL16Z256M4-Codewarrior-setup-quot-vague-quot-error-Which-name/m-p/412161#M11640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With Multylink programmer connected to Freescale MCU KL16Z256M4, an error is reported back&amp;nbsp; in Hardware Connection&amp;gt;&amp;gt;Advanced Programming Options:&amp;nbsp; "Device name could not be determined". &lt;/P&gt;&lt;P&gt;Which name? Is just the name it's missing? Never had seen this error!&lt;/P&gt;&lt;P&gt;Setup settings and MCU are ok since it work correctly on different machines. Any clue for this "vague" error.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;David Palma&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2015 16:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/KL16Z256M4-Codewarrior-setup-quot-vague-quot-error-Which-name/m-p/412161#M11640</guid>
      <dc:creator>djmp</dc:creator>
      <dc:date>2015-09-25T16:45:20Z</dc:date>
    </item>
    <item>
      <title>Re:  KL16Z256M4 Codewarrior setup "vague" error: Which name?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/KL16Z256M4-Codewarrior-setup-quot-vague-quot-error-Which-name/m-p/412162#M11641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you use CW for MCU V10.6 ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Else what is the tool version ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CW for MCU v10.6.4 is the last version.&lt;/P&gt;&lt;P&gt;A patch V10.6.5 can be installed too.&lt;/P&gt;&lt;P&gt;The P&amp;amp;E interfaces Mulitlink are supported by this configuration.&lt;/P&gt;&lt;P&gt;Now it could be important to know exactly the name of interface and rev.&lt;/P&gt;&lt;P&gt;There are several Multilink interfaces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To test it I recommend to create a sample project (project Wizard) for your hardware configuration.&lt;/P&gt;&lt;P&gt;With this example, you should be able to load the example on board without problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Sep 2015 12:32:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/KL16Z256M4-Codewarrior-setup-quot-vague-quot-error-Which-name/m-p/412162#M11641</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-09-28T12:32:36Z</dc:date>
    </item>
  </channel>
</rss>