<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 MK70 UART Module clock</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/MK70-UART-Module-clock/m-p/409739#M11621</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am in the process of setting up the UART Baud on an MK70FN1M0VMJ12 (custom board). I need to know how to verify/set the Module Clock frequency. It seems this is derived from the Bus clock yet I have not found a register to set or verify for the frequency.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 May 2015 19:02:04 GMT</pubDate>
    <dc:creator>codybennett</dc:creator>
    <dc:date>2015-05-07T19:02:04Z</dc:date>
    <item>
      <title>MK70 UART Module clock</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/MK70-UART-Module-clock/m-p/409739#M11621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am in the process of setting up the UART Baud on an MK70FN1M0VMJ12 (custom board). I need to know how to verify/set the Module Clock frequency. It seems this is derived from the Bus clock yet I have not found a register to set or verify for the frequency.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 May 2015 19:02:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/MK70-UART-Module-clock/m-p/409739#M11621</guid>
      <dc:creator>codybennett</dc:creator>
      <dc:date>2015-05-07T19:02:04Z</dc:date>
    </item>
    <item>
      <title>Re: MK70 UART Module clock</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/MK70-UART-Module-clock/m-p/409740#M11622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9447i75455B751967461B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;so , you should be sure the number of UART.&lt;/P&gt;&lt;P&gt;Then we can refer to the clocking didagram calculate the system clock or&amp;nbsp; bus clock , please see :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9579i0F76A7813B449884/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And each part can be found the related register on the RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2015 01:55:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/MK70-UART-Module-clock/m-p/409740#M11622</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-05-13T01:55:55Z</dc:date>
    </item>
  </channel>
</rss>