<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックDebugger broken for assembly</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Debugger-broken-for-assembly/m-p/385973#M11428</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've lost the ability to single step with the debugger in CW10.6, XP-SP3, 9S08SH16 target, Pemicro USBML-Universal. I've re-installed CW10.6 to no avail.&lt;/P&gt;&lt;P&gt;I can step with the debugger, and at times, it jumps to some arbitrary location. Note: NO INTERRUPTS on the target are enabled. When I do single step, it behaves correctly - most of the time&lt;/P&gt;&lt;P&gt;except for the previously cited jump to oblivion. However, when I run the code and then inspect buffers to verify data integrity - nada - it's all 0's. It's as if the debugger pod is not even retrieving data or updating the views at the breakpoint.&lt;/P&gt;&lt;P&gt;Furthermore, when I force an update - nothing. I've already lost 2 days on this and I cannot afford to lose any more time. Has anyone else had this much trouble with the debugger?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Aug 2014 00:57:30 GMT</pubDate>
    <dc:creator>bob_walker</dc:creator>
    <dc:date>2014-08-28T00:57:30Z</dc:date>
    <item>
      <title>Debugger broken for assembly</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Debugger-broken-for-assembly/m-p/385973#M11428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've lost the ability to single step with the debugger in CW10.6, XP-SP3, 9S08SH16 target, Pemicro USBML-Universal. I've re-installed CW10.6 to no avail.&lt;/P&gt;&lt;P&gt;I can step with the debugger, and at times, it jumps to some arbitrary location. Note: NO INTERRUPTS on the target are enabled. When I do single step, it behaves correctly - most of the time&lt;/P&gt;&lt;P&gt;except for the previously cited jump to oblivion. However, when I run the code and then inspect buffers to verify data integrity - nada - it's all 0's. It's as if the debugger pod is not even retrieving data or updating the views at the breakpoint.&lt;/P&gt;&lt;P&gt;Furthermore, when I force an update - nothing. I've already lost 2 days on this and I cannot afford to lose any more time. Has anyone else had this much trouble with the debugger?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Aug 2014 00:57:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Debugger-broken-for-assembly/m-p/385973#M11428</guid>
      <dc:creator>bob_walker</dc:creator>
      <dc:date>2014-08-28T00:57:30Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger broken for assembly</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Debugger-broken-for-assembly/m-p/385974#M11429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello Bob.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this problem has to be checked with your project,&amp;nbsp; please upload it here, we can check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Zhang Jun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Sep 2014 02:57:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Debugger-broken-for-assembly/m-p/385974#M11429</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-09-02T02:57:01Z</dc:date>
    </item>
  </channel>
</rss>