<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: structure of afx-file?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/structure-of-afx-file/m-p/375211#M11386</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is a standard ELF/Dwarf (&lt;A href="http://en.wikipedia.org/wiki/DWARF" title="http://en.wikipedia.org/wiki/DWARF"&gt;DWARF - Wikipedia, the free encyclopedia&lt;/A&gt;) file, just with the .afx extension instead of .elf.&lt;/P&gt;&lt;P&gt;You can see this if you open the file with a text editor and if you look at the first few bytes.&lt;/P&gt;&lt;P&gt;So you should be able to use any tools which accept an ELF file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Sep 2014 12:48:54 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2014-09-17T12:48:54Z</dc:date>
    <item>
      <title>structure of afx-file?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/structure-of-afx-file/m-p/375210#M11385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I'd like to understand the structure of the afx-file.&lt;/P&gt;&lt;P&gt;As far as I have found, it contains the executable code plus the symols for debugging.&lt;/P&gt;&lt;P&gt;But I did not find a documentation of the file structure.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'd like to extract the executable code from the afx rather than decoding from an S19 file.&lt;/P&gt;&lt;P&gt;Furthermore I would like to extract information like the base address.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 12:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/structure-of-afx-file/m-p/375210#M11385</guid>
      <dc:creator>martinpi</dc:creator>
      <dc:date>2014-09-17T12:33:37Z</dc:date>
    </item>
    <item>
      <title>Re: structure of afx-file?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/structure-of-afx-file/m-p/375211#M11386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is a standard ELF/Dwarf (&lt;A href="http://en.wikipedia.org/wiki/DWARF" title="http://en.wikipedia.org/wiki/DWARF"&gt;DWARF - Wikipedia, the free encyclopedia&lt;/A&gt;) file, just with the .afx extension instead of .elf.&lt;/P&gt;&lt;P&gt;You can see this if you open the file with a text editor and if you look at the first few bytes.&lt;/P&gt;&lt;P&gt;So you should be able to use any tools which accept an ELF file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 12:48:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/structure-of-afx-file/m-p/375211#M11386</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-09-17T12:48:54Z</dc:date>
    </item>
  </channel>
</rss>