<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to modify project options after it is created in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-modify-project-options-after-it-is-created/m-p/342572#M11180</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi SL,&lt;/P&gt;&lt;P&gt;see &lt;A href="http://mcuoneclipse.com/2013/02/07/tutorial-printf-with-and-without-processor-expert/" title="http://mcuoneclipse.com/2013/02/07/tutorial-printf-with-and-without-processor-expert/"&gt;Tutorial: Printf() with (and without) Processor Expert | MCU on Eclipse&lt;/A&gt; which shows which of the library and I/O options end up as project settings.&lt;/P&gt;&lt;P&gt;With this, you can easily modify your selection after the project has been created.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 15 Nov 2014 14:41:03 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2014-11-15T14:41:03Z</dc:date>
    <item>
      <title>How to modify project options after it is created</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-modify-project-options-after-it-is-created/m-p/342571#M11179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When one creates a new MCU project in CodeWarrior (10.x), CodeWarrior asks the user to configure the project. For example, it asks the user whether Rapid Code Creation is needed or options for I/O (for the "printf" command). How can the user modify these selections after the project is created? &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I chose "console" as the I/O for "printf" when creating a project, and this is pretty handy for displaying some messages or values in the console window in debug mode. The drawback is that the the firmware cannot run standalone. It relies on the debugger to run. When debugging is done, I need to disable "I/O" (not the pin GPIO) so that the firmware can run by itself. How can I modify the project options without creating a new project from scratch? Thank you.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--SL &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Nov 2014 23:34:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-modify-project-options-after-it-is-created/m-p/342571#M11179</guid>
      <dc:creator>shouminliu</dc:creator>
      <dc:date>2014-11-14T23:34:22Z</dc:date>
    </item>
    <item>
      <title>Re: How to modify project options after it is created</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-modify-project-options-after-it-is-created/m-p/342572#M11180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi SL,&lt;/P&gt;&lt;P&gt;see &lt;A href="http://mcuoneclipse.com/2013/02/07/tutorial-printf-with-and-without-processor-expert/" title="http://mcuoneclipse.com/2013/02/07/tutorial-printf-with-and-without-processor-expert/"&gt;Tutorial: Printf() with (and without) Processor Expert | MCU on Eclipse&lt;/A&gt; which shows which of the library and I/O options end up as project settings.&lt;/P&gt;&lt;P&gt;With this, you can easily modify your selection after the project has been created.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Nov 2014 14:41:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/How-to-modify-project-options-after-it-is-created/m-p/342572#M11180</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-11-15T14:41:03Z</dc:date>
    </item>
  </channel>
</rss>