<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: Generate Full Disassembly Listing in CW3.1 for HCS12</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Generate-Full-Disassembly-Listing-in-CW3-1-for-HCS12/m-p/131138#M1117</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Both the *.s19 and the *.phy are usually SRecord files with no debug information. They usually differ in the addresses used in them.&lt;BR /&gt;&lt;BR /&gt;As CW does not support to produce those files without an abs/elf file, I'm pretty sure you have one :smileyhappy:. However the extension can be choosen, so maybe someone did pick something else in your project. The directory for the abs/elf file can be configured in the Target Settings the "Output Directory" field. The filename is configured in the "Linker for HC12" preference page, "Application Filename" field.&lt;BR /&gt;&lt;BR /&gt;In standard projects the abs/elf file is placed in a bin subfolder and has a *.abs extension.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Sep 2006 03:38:14 GMT</pubDate>
    <dc:creator>CompilerGuru</dc:creator>
    <dc:date>2006-09-26T03:38:14Z</dc:date>
    <item>
      <title>Generate Full Disassembly Listing in CW3.1 for HCS12</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Generate-Full-Disassembly-Listing-in-CW3-1-for-HCS12/m-p/131135#M1114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am using CodeWarrior for HC(S)12 v.3.1 for Windows. I am trying to generate a full disassembly listing of my entire project that includes symbols.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have opened the Decoder (decoder.exe) utility separately from the IDE and have been able to disassemble the .s19 file that is created when I compile. That disassembly does seem to be for the whole project; however, it doesn't have any debug information (i.e. the symbol names, etc.) in it. Is there a way to have the decoder generate this type of file with the extra debug information?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;(Inside the IDE, I can click on any 1 .c file and right-click and pick "Disassemble". This produces a nice disassembly of that file, with symbols, but I'd like it for the whole project to aid in off-line debugging.)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Finally, I noticed that the Decoder can use .elf, .abs, and .lib files for input. Would any of these do what I want? If so, how do I have the IDE create these files when I compile?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-- Greg&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Sep 2006 00:50:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Generate-Full-Disassembly-Listing-in-CW3-1-for-HCS12/m-p/131135#M1114</guid>
      <dc:creator>tocard</dc:creator>
      <dc:date>2006-09-23T00:50:26Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Full Disassembly Listing in CW3.1 for HCS12</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Generate-Full-Disassembly-Listing-in-CW3-1-for-HCS12/m-p/131136#M1115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Check the thread "Generate a Full listing files" which was about exactly the same topic.&lt;BR /&gt;&lt;BR /&gt;It was for HC08 V5.1, but the same aplies to HC12 V3.1.&lt;BR /&gt;Daniel&lt;BR /&gt;&lt;BR /&gt;PS: decode the abs.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Sep 2006 06:00:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Generate-Full-Disassembly-Listing-in-CW3-1-for-HCS12/m-p/131136#M1115</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2006-09-23T06:00:28Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Full Disassembly Listing in CW3.1 for HCS12</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Generate-Full-Disassembly-Listing-in-CW3-1-for-HCS12/m-p/131137#M1116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thank you CompilerGuru.&lt;BR /&gt;&lt;BR /&gt;I had originally started with the "Generate a Full listing files" post in my search before I posted. However, that thread suggests using the .abs file, which you also mentioned. I do not have a file with that extension and I can't see a way to generate it, either.&lt;BR /&gt;&lt;BR /&gt;When I compile, CW creates a .s19 and a .phy file. Are either of these equivalent? If not, how do I compile my project to create a .abs file as well?&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Sep 2006 20:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Generate-Full-Disassembly-Listing-in-CW3-1-for-HCS12/m-p/131137#M1116</guid>
      <dc:creator>tocard</dc:creator>
      <dc:date>2006-09-25T20:31:33Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Full Disassembly Listing in CW3.1 for HCS12</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Generate-Full-Disassembly-Listing-in-CW3-1-for-HCS12/m-p/131138#M1117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Both the *.s19 and the *.phy are usually SRecord files with no debug information. They usually differ in the addresses used in them.&lt;BR /&gt;&lt;BR /&gt;As CW does not support to produce those files without an abs/elf file, I'm pretty sure you have one :smileyhappy:. However the extension can be choosen, so maybe someone did pick something else in your project. The directory for the abs/elf file can be configured in the Target Settings the "Output Directory" field. The filename is configured in the "Linker for HC12" preference page, "Application Filename" field.&lt;BR /&gt;&lt;BR /&gt;In standard projects the abs/elf file is placed in a bin subfolder and has a *.abs extension.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2006 03:38:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Generate-Full-Disassembly-Listing-in-CW3-1-for-HCS12/m-p/131138#M1117</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2006-09-26T03:38:14Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Full Disassembly Listing in CW3.1 for HCS12</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Generate-Full-Disassembly-Listing-in-CW3-1-for-HCS12/m-p/131139#M1118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Yes, that was it. I looked in the Project Options and found that the "Application Name" did not have an extension at all. When I decoded that extensionless file, everything worked as you said. The decoder even noted that is was an ELF/DWARF encoded file.&lt;BR /&gt;&lt;BR /&gt;(My guess is that it was named without the .abs so that the .phy and .s19 files would have the name "&lt;I&gt;project_name&lt;/I&gt;.s19" instead of "&lt;I&gt;project_name&lt;/I&gt;.abs.s19".)&lt;BR /&gt;&lt;BR /&gt;Thanks again!&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Sep 2006 00:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Generate-Full-Disassembly-Listing-in-CW3-1-for-HCS12/m-p/131139#M1118</guid>
      <dc:creator>tocard</dc:creator>
      <dc:date>2006-09-27T00:23:54Z</dc:date>
    </item>
  </channel>
</rss>