<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CW 10.6 Debug Error in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-6-Debug-Error/m-p/340891#M11168</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What happens is this:&lt;/P&gt;&lt;P&gt;the burner.exe uses the "Accelerometer.abs.args" file (can you post its content?) as command line option and executes the burner.bbl file (can you post that content too?).&lt;/P&gt;&lt;P&gt;It seems that it tries to read/open the AccelerometerTest.s19 file (which sounds wrong, as this is the output file, and it should use the *.abs or *.elf as input).&lt;/P&gt;&lt;P&gt;Posting your .bbl and .args hopefully will show what the problem is.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Feb 2015 20:09:10 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2015-02-02T20:09:10Z</dc:date>
    <item>
      <title>CW 10.6 Debug Error</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-6-Debug-Error/m-p/340890#M11167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been handed an HC08QE8-based Codewarrior project to take over.&amp;nbsp; Unfortunately, it was poorly managed and I am a CodeWarrior amateur.&amp;nbsp;&amp;nbsp; I am able to build the project, but when it attempts to download via P&amp;amp;E USB multilink Universal (Rev A), burner outputs an error that it can't find "AccelerometerTest.s19".&amp;nbsp; The issue is that the file doesn't exist because the file generated is "Accelerometer.s19".&amp;nbsp; I have searched through Project Settings, Build Settings, and Debug Settings, but can find no reference to "AcelerometerTest.s19".&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have attached a screen shot of the CodeWarrior output.&amp;nbsp; Any help is much appreciated.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120163i3955974091AF13A0/image-size/large?v=v2&amp;amp;px=999" title="19391_19391.jpg" alt="19391_19391.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50137i9A758DA263D5A960/image-size/large?v=v2&amp;amp;px=999" title="codewarrior error.jpg" alt="codewarrior error.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2015 17:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-6-Debug-Error/m-p/340890#M11167</guid>
      <dc:creator>bryano</dc:creator>
      <dc:date>2015-02-02T17:56:06Z</dc:date>
    </item>
    <item>
      <title>Re: CW 10.6 Debug Error</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-6-Debug-Error/m-p/340891#M11168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What happens is this:&lt;/P&gt;&lt;P&gt;the burner.exe uses the "Accelerometer.abs.args" file (can you post its content?) as command line option and executes the burner.bbl file (can you post that content too?).&lt;/P&gt;&lt;P&gt;It seems that it tries to read/open the AccelerometerTest.s19 file (which sounds wrong, as this is the output file, and it should use the *.abs or *.elf as input).&lt;/P&gt;&lt;P&gt;Posting your .bbl and .args hopefully will show what the problem is.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2015 20:09:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CW-10-6-Debug-Error/m-p/340891#M11168</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-02-02T20:09:10Z</dc:date>
    </item>
  </channel>
</rss>