<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: Forcing compiler to always compile source</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131108#M1109</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks for your reply.&lt;BR /&gt;&lt;BR /&gt;I'm not sure what you are suggesting, that I should use burner.exe in some way? I wish to avoid external programs, otherwise I could simply write a Windows prog that runs in the background and opens/saves the source file with the date every 10 minutes or so, since CW senses that the file has been changed by another program.&lt;BR /&gt;&lt;BR /&gt;I was just wondering if there was any built-in support for this, since it must be a rather common wish to include compile/linking date info into one's program.&lt;BR /&gt;&lt;BR /&gt;(And yep, I've got the variable in ENTRIES. The linker will pick an old date though, unless changes are made to the .obj file associated with the C file containing the date.)&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Sep 2006 15:07:56 GMT</pubDate>
    <dc:creator>Lundin</dc:creator>
    <dc:date>2006-09-25T15:07:56Z</dc:date>
    <item>
      <title>HC12: Forcing compiler to always compile source</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131106#M1107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I have a constant string in ROM containing the ANSI C constant __DATE__. I want to have the the file containing this constant to be automatically compiled every time I link the project, to get a relevant date code. Is this possible in some way? I don't wish to manually click on the file in the project window, since it is easy to forget.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Or is there another way to get a date stamp downloaded to the flash automatically?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using CW3.1 for HCS12.&lt;/SPAN&gt;&lt;P&gt;Message Edited by CrasyCat on &lt;SPAN class="date_text"&gt;2007-04-13&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;01:55 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Sep 2006 21:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131106#M1107</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2006-09-22T21:48:37Z</dc:date>
    </item>
    <item>
      <title>Re: Forcing compiler to always compile source</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131107#M1108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I think there is a batch burner postlinker plugin in&lt;BR /&gt;HC12 V3.1 (not 100% sure).&lt;BR /&gt;You could use a batch file like this:&lt;BR /&gt;&lt;BR /&gt;echo // automatically generated date &amp;gt; date.c&lt;BR /&gt;echo const char date= "%DATE%"; &amp;gt;&amp;gt; date.c&lt;BR /&gt;&lt;BR /&gt;(and then add ENTRIES date END to the prm file so it gets linked.&lt;BR /&gt;Daniel&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Sep 2006 06:06:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131107#M1108</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2006-09-23T06:06:59Z</dc:date>
    </item>
    <item>
      <title>Re: Forcing compiler to always compile source</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131108#M1109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks for your reply.&lt;BR /&gt;&lt;BR /&gt;I'm not sure what you are suggesting, that I should use burner.exe in some way? I wish to avoid external programs, otherwise I could simply write a Windows prog that runs in the background and opens/saves the source file with the date every 10 minutes or so, since CW senses that the file has been changed by another program.&lt;BR /&gt;&lt;BR /&gt;I was just wondering if there was any built-in support for this, since it must be a rather common wish to include compile/linking date info into one's program.&lt;BR /&gt;&lt;BR /&gt;(And yep, I've got the variable in ENTRIES. The linker will pick an old date though, unless changes are made to the .obj file associated with the C file containing the date.)&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Sep 2006 15:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131108#M1109</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2006-09-25T15:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: Forcing compiler to always compile source</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131109#M1110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Oh I used the wrong word.&lt;BR /&gt;I intended to say "batch runner postlinker". The burner.exe wont help much here.&lt;BR /&gt;Basically in the Target-&amp;gt;Settings, in the Pre-linker or Post-linker tab you can choose to run additional tools, there is a BatchRunner PostLinker , which basically will execute a batch file after every linking phase.&lt;BR /&gt;&lt;BR /&gt;Using the cmd file I preposed below is actually not the right thing, when I think about it as it would encode the data of when you last built the app in future builds, so it would always be off by invocation, so for example the batch file could touch the *.c file containing the __DATE__ macro.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Sep 2006 19:16:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131109#M1110</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2006-09-25T19:16:37Z</dc:date>
    </item>
    <item>
      <title>Re: Forcing compiler to always compile source</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131110#M1111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I think it might work if I delete the .o file associated with the .c file at the same time. I will give it a try, thanks for helping! &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2006 20:17:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131110#M1111</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2006-09-26T20:17:32Z</dc:date>
    </item>
    <item>
      <title>Re: Forcing compiler to always compile source</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131111#M1112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi There,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am trying to achieve this too - so that each time the build is remade, a new time / date / version stamp is created automatically.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;My intial thought was to create a DOS batch file that touched my file containing defines that had the __DATE__ &amp;amp; __TIME__ pragmas, thus forcing creation of a new string.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have been trying to find a way to hook this into codewarriors build process - and it has been suggested, as on this thread (sorry - not sure how to post cross links to other threads - but I have a thread under Codewarrior general - search for "AutoTouch") , that the Post Linker is the way to go. However, the big problem with this is that the compilation has already taken place by this time, and so there needs to be a way to re-kick off a compilation - I assume there is a command line command to perform this but I haven't had the time to search for this!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Of course, this then means that anytime the "Debug" arrow is pressed, a new time and date build string is generated. This is not quite ideal - really what is needed is for the file to be touched only if the compiler has been run (i.e. code has changed). Is there a way of achieving this?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Many Thanks,&lt;/DIV&gt;&lt;DIV&gt;Mike&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Sep 2007 15:09:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131111#M1112</guid>
      <dc:creator>EmbeddedCoder</dc:creator>
      <dc:date>2007-09-03T15:09:43Z</dc:date>
    </item>
    <item>
      <title>Re: Forcing compiler to always compile source</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131112#M1113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While this may be counter intuitive, the trick I am using is to delete the object file with the BatchRunner PostLinker.&amp;nbsp; This guarentees that the next time you Make the project the C file will be compiled and __DATE__ &amp;amp; __TIME__ will be updated.&lt;BR /&gt;&lt;BR /&gt;Here is the contents of my PostLink.bat file&lt;BR /&gt;&lt;BR /&gt;cd %CD%\..\Main_Data\Standard\ObjectCode&lt;BR /&gt;del SysInfo.c.o&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2011 21:56:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/HC12-Forcing-compiler-to-always-compile-source/m-p/131112#M1113</guid>
      <dc:creator>RoyAtRce</dc:creator>
      <dc:date>2011-04-27T21:56:58Z</dc:date>
    </item>
  </channel>
</rss>