<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: Processor Expert</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319144#M10982</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeff,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hum ...&lt;/P&gt;&lt;P&gt;It seems the readme file is not existing anymore and don't know if it was really included in the past.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now to add Procesor Expert in existing project you must:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; File + New + Other...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Processor Expert -&amp;gt; Enable processor expert for existing c project&lt;/P&gt;&lt;P&gt;Then PE will be added in the project ... but&lt;/P&gt;&lt;P&gt;+++++++++++++++++++++++++&lt;/P&gt;&lt;P&gt;Warning&lt;/P&gt;&lt;P&gt;Note that in most cases this conversion involves necessary&lt;/P&gt;&lt;P&gt;manual changes in the application code, because for example&lt;/P&gt;&lt;P&gt;the register interrupt vectors table definitions created by the&lt;/P&gt;&lt;P&gt;user often conflicts with Processor Expert definitions. Don't&lt;/P&gt;&lt;P&gt;forget to backup the whole project before the conversion. Some&lt;/P&gt;&lt;P&gt;files will have to be removed from the project. The conversion&lt;/P&gt;&lt;P&gt;to Processor Expert is recommended to experienced users only.&lt;/P&gt;&lt;P&gt;+++++++++++++++++++++++++&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are more information in the ProcessorExpertHelp.pdf manual&lt;/P&gt;&lt;P&gt;Page 163 the chapter "3.7 Converting project to use Processor Expert"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jun 2014 13:17:21 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2014-06-17T13:17:21Z</dc:date>
    <item>
      <title>Processor Expert</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319137#M10975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been using CW v10.5 for sometime but up until now only editing older code which allows me access to the processor hardware through PE . Today I have started a new project and to my dismay I cannot select Project Expert, the selection button is greyed out when I try to make a new project .. and I get this cryptic message to see readme.txt under project.&lt;/P&gt;&lt;P&gt;Could someone tell me the trick to enabling PE please .. Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Jun 2014 05:10:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319137#M10975</guid>
      <dc:creator>Jep</dc:creator>
      <dc:date>2014-06-14T05:10:36Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319138#M10976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeff,&lt;/P&gt;&lt;P&gt;can you post that message?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Jun 2014 05:40:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319138#M10976</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-06-14T05:40:53Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319139#M10977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erich&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;I have attached a screen grab of the popup that occurs during the project creation.&lt;/P&gt;&lt;P&gt;As you can see it wont allow me to select PE and the message at the bottom is useless.&lt;/P&gt;&lt;P&gt;OK, just noticed this error in the problems tab about processor expert .. no license .. I dont understand&lt;/P&gt;&lt;P&gt;I thought PE came with this Special suite that I use .. well it did with all of the others.&lt;/P&gt;&lt;P&gt;I really hope that you can steer me in the right direction.&lt;/P&gt;&lt;P&gt;Oh and by the way I downloaded the latest CW Eclipse SE V10.6 and am using that now .. well trying to&amp;nbsp; &lt;/P&gt;&lt;P&gt;Thanks again&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="CW capture.JPG.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41885iEE5F216C6B2F3C76/image-size/large?v=v2&amp;amp;px=999" role="button" title="CW capture.JPG.jpg" alt="CW capture.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="CW2 capture.JPG.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42197iD80451D95E3881A5/image-size/large?v=v2&amp;amp;px=999" role="button" title="CW2 capture.JPG.jpg" alt="CW2 capture.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jun 2014 00:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319139#M10977</guid>
      <dc:creator>Jep</dc:creator>
      <dc:date>2014-06-16T00:51:59Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319140#M10978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeff,&lt;/P&gt;&lt;P&gt;for which microcontroller you want to create a project? If that option is grayed out, it seems that it is not supported by Processor Expert for some reason.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jun 2014 04:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319140#M10978</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-06-16T04:06:34Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319141#M10979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the MC9S08SH8 and the MC9S08AC32 mostly in my designs .. when I start a new project CW certainly gives me the option of selecting these processors.&lt;/P&gt;&lt;P&gt;It all worked fabulously until I upgraded to V10.5 I guess I just didnt know as I had only ever made changes to code from when I had upgraded not actually started a new project.&lt;/P&gt;&lt;P&gt;So what do you make of the message seeing the readme txt to find out how to enable PE ??&lt;/P&gt;&lt;P&gt;Also I use assembler to program .. dont know if that makes a difference now&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help because I have a getting urgent project to start&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards Jeff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jun 2014 03:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319141#M10979</guid>
      <dc:creator>Jep</dc:creator>
      <dc:date>2014-06-17T03:16:29Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319142#M10980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeff,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've 2 versions:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCU V10.5 and MCU V10.6&lt;/P&gt;&lt;P&gt;To be running each installation must be done on a specific folder for instance:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; C:\Freescale\CW MCU v10.5&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; C:\Freescale\CW MCU v10.6&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Under these 2 versions I'm able to create the project for S08SH8 and S08AC32 with Processor Expert.&lt;/P&gt;&lt;P&gt;Now if you select Relocatable Assembly source code only -&amp;gt; this means un-check C, the Processor Expert can not be selected anymore.&lt;/P&gt;&lt;P&gt;Processor Expert generates C code only and not assembly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jun 2014 11:51:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319142#M10980</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-06-17T11:51:08Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319143#M10981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pascal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So are you telling me that I cannot use processor expert if I select relocatable or absolute assembler ... OK&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="CW capture.JPG.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43078i24C5BEC0FB81309E/image-size/large?v=v2&amp;amp;px=999" role="button" title="CW capture.JPG.jpg" alt="CW capture.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Please look again at this picture and the the message in the box above&lt;/P&gt;&lt;P&gt;"No device initialization code is generated. Only generates start up code. See readme.txt in project how Processor Expert can be enabled (If not done here)&lt;/P&gt;&lt;P&gt;So Pascal .. where is this readme.txt file located .. Ive tried .. but you are the guru .. over to you&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;JEff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jun 2014 12:06:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319143#M10981</guid>
      <dc:creator>Jep</dc:creator>
      <dc:date>2014-06-17T12:06:55Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319144#M10982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeff,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hum ...&lt;/P&gt;&lt;P&gt;It seems the readme file is not existing anymore and don't know if it was really included in the past.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now to add Procesor Expert in existing project you must:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; File + New + Other...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Processor Expert -&amp;gt; Enable processor expert for existing c project&lt;/P&gt;&lt;P&gt;Then PE will be added in the project ... but&lt;/P&gt;&lt;P&gt;+++++++++++++++++++++++++&lt;/P&gt;&lt;P&gt;Warning&lt;/P&gt;&lt;P&gt;Note that in most cases this conversion involves necessary&lt;/P&gt;&lt;P&gt;manual changes in the application code, because for example&lt;/P&gt;&lt;P&gt;the register interrupt vectors table definitions created by the&lt;/P&gt;&lt;P&gt;user often conflicts with Processor Expert definitions. Don't&lt;/P&gt;&lt;P&gt;forget to backup the whole project before the conversion. Some&lt;/P&gt;&lt;P&gt;files will have to be removed from the project. The conversion&lt;/P&gt;&lt;P&gt;to Processor Expert is recommended to experienced users only.&lt;/P&gt;&lt;P&gt;+++++++++++++++++++++++++&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are more information in the ProcessorExpertHelp.pdf manual&lt;/P&gt;&lt;P&gt;Page 163 the chapter "3.7 Converting project to use Processor Expert"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jun 2014 13:17:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319144#M10982</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-06-17T13:17:21Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319145#M10983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Pascal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This information doesnt really help. I have told you I dont program in C ..&lt;/P&gt;&lt;P&gt;The software WONT ALLOW me to add processor expert.&lt;/P&gt;&lt;P&gt;These steps&lt;/P&gt;&lt;P&gt;Now to add Procesor Expert in existing project you must:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; File + New + Other...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Processor Expert -&amp;gt; Enable processor expert for existing project&lt;/P&gt;&lt;P&gt;CANT be done in an assembler project .. ALL options to enable it are greyed out&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I dont need to know how to add PE to a C project because I dont program in C and if I did I would simply select PE at the start.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jun 2014 00:16:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319145#M10983</guid>
      <dc:creator>Jep</dc:creator>
      <dc:date>2014-06-18T00:16:11Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Processor Expert</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319146#M10984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeff,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Processor Expert generates code in C only.&lt;/P&gt;&lt;P&gt;So adding PE&amp;nbsp; which includes C code only in Assembly project is it really interesting ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However on my MCU V10.6 I can add Processor Expert in an application created for Relocatable Assembly only.&lt;/P&gt;&lt;P&gt;Now is it really usable ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I don't think - You need to change the main.asm file ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think the better solution is to add PE in a mixed C and Relocatable Assembly project.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jun 2014 05:22:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Processor-Expert/m-p/319146#M10984</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-06-18T05:22:40Z</dc:date>
    </item>
  </channel>
</rss>