<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic where is defined  extern uint32_t __SP_INIT; in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/where-is-defined-extern-uint32-t-SP-INIT/m-p/307848#M10858</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, sorry for my banal question. I'm using codewarrior for kinetis kl15. Where is define&amp;nbsp; extern uint32_t __SP_INIT;&lt;/P&gt;&lt;P&gt;I see sp=0x20003000 but where can I see this setting?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Apr 2014 16:38:55 GMT</pubDate>
    <dc:creator>stefanomanca</dc:creator>
    <dc:date>2014-04-01T16:38:55Z</dc:date>
    <item>
      <title>where is defined  extern uint32_t __SP_INIT;</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/where-is-defined-extern-uint32-t-SP-INIT/m-p/307848#M10858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, sorry for my banal question. I'm using codewarrior for kinetis kl15. Where is define&amp;nbsp; extern uint32_t __SP_INIT;&lt;/P&gt;&lt;P&gt;I see sp=0x20003000 but where can I see this setting?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2014 16:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/where-is-defined-extern-uint32-t-SP-INIT/m-p/307848#M10858</guid>
      <dc:creator>stefanomanca</dc:creator>
      <dc:date>2014-04-01T16:38:55Z</dc:date>
    </item>
    <item>
      <title>Re: where is defined  extern uint32_t __SP_INIT;</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/where-is-defined-extern-uint32-t-SP-INIT/m-p/307849#M10859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Stefano:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Never feel sorry about a question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The __SP_INIT symbol is declared and initialized in the linker file (e.g. &lt;STRONG&gt;MKL15Z128_flash.ld&lt;/STRONG&gt;). There you will find something like the next:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="plain" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_13963756566359192" jivemacro_uid="_13963756566359192" modifiedtitle="true"&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;/* Highest address of the user mode stack */&lt;/P&gt;
&lt;P&gt;_estack = 0x20003000;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* end of SRAM */&lt;/P&gt;
&lt;P&gt;__SP_INIT = _estack;&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;

&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2014 18:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/where-is-defined-extern-uint32-t-SP-INIT/m-p/307849#M10859</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-04-01T18:08:37Z</dc:date>
    </item>
  </channel>
</rss>