<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Incorrect toolchain selected, CW10.6.</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Incorrect-toolchain-selected-CW10-6/m-p/304157#M10813</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using Codewarrior 10.6. The processor is MK20DX128VLH7, 64 pin package. Using Processor expert, C code, No I/O, ARM Toolchain when creating the project.&lt;/P&gt;&lt;P&gt;Creating a new project only provides for the 100 pin variant to choose from. I added the 64 pin part from the processor expert, this is when I get the message "Incorrect toolchain selected in the project settings. Please change your project setting to use 'ARM Toolchain' or change the selected Compiler".&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I get the 64pin package to use the same Toolchain?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 May 2014 14:11:15 GMT</pubDate>
    <dc:creator>randenewberry</dc:creator>
    <dc:date>2014-05-23T14:11:15Z</dc:date>
    <item>
      <title>Incorrect toolchain selected, CW10.6.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Incorrect-toolchain-selected-CW10-6/m-p/304157#M10813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using Codewarrior 10.6. The processor is MK20DX128VLH7, 64 pin package. Using Processor expert, C code, No I/O, ARM Toolchain when creating the project.&lt;/P&gt;&lt;P&gt;Creating a new project only provides for the 100 pin variant to choose from. I added the 64 pin part from the processor expert, this is when I get the message "Incorrect toolchain selected in the project settings. Please change your project setting to use 'ARM Toolchain' or change the selected Compiler".&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I get the 64pin package to use the same Toolchain?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 May 2014 14:11:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Incorrect-toolchain-selected-CW10-6/m-p/304157#M10813</guid>
      <dc:creator>randenewberry</dc:creator>
      <dc:date>2014-05-23T14:11:15Z</dc:date>
    </item>
    <item>
      <title>Re: Incorrect toolchain selected, CW10.6.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Incorrect-toolchain-selected-CW10-6/m-p/304158#M10814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tired on CW10.6, but did not reproduce the problem. Did you select the same options with me?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Untitled.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43755i9638570CAD94449C/image-size/large?v=v2&amp;amp;px=999" role="button" title="Untitled.png" alt="Untitled.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached the project which I have changed the CPU into 64-pin MK20DX128VLH7. It built well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 May 2014 03:31:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Incorrect-toolchain-selected-CW10-6/m-p/304158#M10814</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2014-05-26T03:31:37Z</dc:date>
    </item>
  </channel>
</rss>