<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: MobileGTv9.2, Ethernet tap, CCSProtocolPlugin: CCS: Connection refused</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/MobileGTv9-2-Ethernet-tap-CCSProtocolPlugin-CCS-Connection/m-p/302136#M10785</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the delay.&lt;/P&gt;&lt;P&gt;I don't have experience with linux version.&lt;/P&gt;&lt;P&gt;However we have the same problem under Windows version.&lt;/P&gt;&lt;P&gt;A colleague worked on solution.&lt;/P&gt;&lt;P&gt;Attached you will find the Note explaining how to install and use the TAP interface under MGT V9.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;!Have a great day,&lt;BR /&gt;Pascal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 May 2014 12:04:47 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2014-05-02T12:04:47Z</dc:date>
    <item>
      <title>MobileGTv9.2, Ethernet tap, CCSProtocolPlugin: CCS: Connection refused</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/MobileGTv9-2-Ethernet-tap-CCSProtocolPlugin-CCS-Connection/m-p/302135#M10784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am attempting to get the latest CW for MobileGT to work on my 64-bit pc running Debian Linux 3.2.54. The target is a MPC5200cvr400B. The CW Ethernet tap is on the network and I can ping it ok. However, when I go to Project-&amp;gt;Debug this window pops up saying the connection is refused. I have double checked the ribbon cable orientation.&lt;/P&gt;&lt;P&gt;Also, I can telnet into the TAP. Any suggestions as to what to look for?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Apr 2014 15:38:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/MobileGTv9-2-Ethernet-tap-CCSProtocolPlugin-CCS-Connection/m-p/302135#M10784</guid>
      <dc:creator>danedmondson</dc:creator>
      <dc:date>2014-04-23T15:38:56Z</dc:date>
    </item>
    <item>
      <title>Re: MobileGTv9.2, Ethernet tap, CCSProtocolPlugin: CCS: Connection refused</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/MobileGTv9-2-Ethernet-tap-CCSProtocolPlugin-CCS-Connection/m-p/302136#M10785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the delay.&lt;/P&gt;&lt;P&gt;I don't have experience with linux version.&lt;/P&gt;&lt;P&gt;However we have the same problem under Windows version.&lt;/P&gt;&lt;P&gt;A colleague worked on solution.&lt;/P&gt;&lt;P&gt;Attached you will find the Note explaining how to install and use the TAP interface under MGT V9.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;!Have a great day,&lt;BR /&gt;Pascal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 May 2014 12:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/MobileGTv9-2-Ethernet-tap-CCSProtocolPlugin-CCS-Connection/m-p/302136#M10785</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-05-02T12:04:47Z</dc:date>
    </item>
    <item>
      <title>Re: MobileGTv9.2, Ethernet tap, CCSProtocolPlugin: CCS: Connection refused</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/MobileGTv9-2-Ethernet-tap-CCSProtocolPlugin-CCS-Connection/m-p/302137#M10786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pascal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for your note. I have, however, settled on the linux version and worked through any issues. The ethernet tap is working pretty well with MobileGT but I can see that we will have a need for a more powerful IDE. Specifically one that can flash a 128M nand without choking, and that can also upload an entire flash image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I left the Windows version, the last issue I was encountering was that MobileGT would not start due to a read/write issue on a configuration file. Even our IT admin could not get that one to work, so I'm happy with the linux version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 May 2014 12:28:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/MobileGTv9-2-Ethernet-tap-CCSProtocolPlugin-CCS-Connection/m-p/302137#M10786</guid>
      <dc:creator>danedmondson</dc:creator>
      <dc:date>2014-05-02T12:28:53Z</dc:date>
    </item>
  </channel>
</rss>