<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: codeworrier debugging without BDM h/w tap</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/codeworrier-debugging-without-BDM-h-w-tap/m-p/284391#M10503</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, I see that if the target board has an integrted or background debugger (which my M52233DEMO does) then the OSBDM s/w (JM60) can be used to perform what I require. Ie debugging on the target h/w (controlled under CodeWarrior IDE) without having to purchase a h/w tap.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I should have done my reading first before posting - hopefully at least someone may read this and be pointed in the right direction! I also just spotted the OSBDM section of this Community Forum - so viewing that &amp;amp; reading the manuals is up next ....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Mar 2013 09:47:11 GMT</pubDate>
    <dc:creator>andrewheywood23</dc:creator>
    <dc:date>2013-03-07T09:47:11Z</dc:date>
    <item>
      <title>codeworrier debugging without BDM h/w tap</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/codeworrier-debugging-without-BDM-h-w-tap/m-p/284390#M10502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have recently purchased 2 development boards. The M5223DEMO coldfire v2 board &amp;amp; I use codeworrier v 7.2 for coldfire MCUs &amp;amp;&lt;/P&gt;&lt;P&gt;MPC885ADS PowerPc (PowerQUICC) board where I use codeworrier v8.8 for power PCs.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was hoping to use the debugger via either the sandard RS232 port or the USB port or even ethernet to perform the debugger functions of comms between the codeworrier IDE &amp;amp; the target development board - but as a direct connection without the use of a hardware BDM tap module.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this possible? within my list of debugger connections I only seems to have PE micro, Abatron entries and they all seem to require h/w tap devices. I understand that without one some debug features won't be possible - but I was hoping that a console I/O type method of debugging would be possible via a simpe RS232 link betweeon codewarrior host and target board &amp;amp; no h/w tap in between.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any pointers would be most appreciated akso appologies if this question has been posted before &amp;amp; I've missed it during my searches.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Mar 2013 22:53:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/codeworrier-debugging-without-BDM-h-w-tap/m-p/284390#M10502</guid>
      <dc:creator>andrewheywood23</dc:creator>
      <dc:date>2013-03-05T22:53:27Z</dc:date>
    </item>
    <item>
      <title>Re: codeworrier debugging without BDM h/w tap</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/codeworrier-debugging-without-BDM-h-w-tap/m-p/284391#M10503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, I see that if the target board has an integrted or background debugger (which my M52233DEMO does) then the OSBDM s/w (JM60) can be used to perform what I require. Ie debugging on the target h/w (controlled under CodeWarrior IDE) without having to purchase a h/w tap.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I should have done my reading first before posting - hopefully at least someone may read this and be pointed in the right direction! I also just spotted the OSBDM section of this Community Forum - so viewing that &amp;amp; reading the manuals is up next ....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2013 09:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/codeworrier-debugging-without-BDM-h-w-tap/m-p/284391#M10503</guid>
      <dc:creator>andrewheywood23</dc:creator>
      <dc:date>2013-03-07T09:47:11Z</dc:date>
    </item>
    <item>
      <title>Re: codeworrier debugging without BDM h/w tap</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/codeworrier-debugging-without-BDM-h-w-tap/m-p/284392#M10504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Excellent observation Andrew, thanks for sharing!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Monica&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2013 00:09:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/codeworrier-debugging-without-BDM-h-w-tap/m-p/284392#M10504</guid>
      <dc:creator>Monica</dc:creator>
      <dc:date>2013-03-14T00:09:38Z</dc:date>
    </item>
  </channel>
</rss>