<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Codewarrior 10.x how to expand several structures at once</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282646#M10464</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Any one know how to open an array of 100 structures quickly in CodeWarrior?&amp;nbsp; Maybe if there isn't a button to do this, is there any macro recording capability?&amp;nbsp; Guess I could get a keyboard that records macros, but I'd rather have the macro built into the tools...&amp;nbsp; 8-&amp;lt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Mar 2013 22:50:05 GMT</pubDate>
    <dc:creator>nmay</dc:creator>
    <dc:date>2013-03-21T22:50:05Z</dc:date>
    <item>
      <title>Codewarrior 10.x how to expand several structures at once</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282645#M10463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an array of 100 structures and when I view the array in the Variables window, all the structures are collapsed.&amp;nbsp; I have to click on each one to expand it.&amp;nbsp; Is there a way to expand all the structures at the same time?&amp;nbsp; It is really cumbersome to expand all these items!&amp;nbsp; I did notice that this was the same issue discussed for an earlier version of CW.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've also noticed that with CodeWarrior 10.3, if when I have the array of 100 structures open (they don't all fit on one screen) and they are selected (with select all).&amp;nbsp; When I right click with the mouse to view them as decimal, only some of them change.&amp;nbsp; Some of the variables on pages I cannot see are still the old display type.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--Norm&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Mar 2013 20:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282645#M10463</guid>
      <dc:creator>nmay</dc:creator>
      <dc:date>2013-03-04T20:37:15Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10.x how to expand several structures at once</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282646#M10464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Any one know how to open an array of 100 structures quickly in CodeWarrior?&amp;nbsp; Maybe if there isn't a button to do this, is there any macro recording capability?&amp;nbsp; Guess I could get a keyboard that records macros, but I'd rather have the macro built into the tools...&amp;nbsp; 8-&amp;lt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2013 22:50:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282646#M10464</guid>
      <dc:creator>nmay</dc:creator>
      <dc:date>2013-03-21T22:50:05Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10.x how to expand several structures at once</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282647#M10465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It looks like this is a long outstanding wish for Eclipse:&lt;/P&gt;&lt;P&gt;&lt;A href="https://bugs.eclipse.org/bugs/show_bug.cgi?id=129787" title="https://bugs.eclipse.org/bugs/show_bug.cgi?id=129787"&gt;https://bugs.eclipse.org/bugs/show_bug.cgi?id=129787&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://bugs.eclipse.org/bugs/show_bug.cgi?id=129787" title="https://bugs.eclipse.org/bugs/show_bug.cgi?id=129787"&gt;https://bugs.eclipse.org/bugs/show_bug.cgi?id=129787&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The concern above is that 'expand all' is not possible because of potentially recursive structs. But it would be feasible to expand all structs just one level.&lt;/P&gt;&lt;P&gt;So bottom line: this has not been implemented (yet?) in Eclipse.&lt;/P&gt;&lt;P&gt;But it should be possible to write a script using the command line debugger (menu Window &amp;gt; Show View &amp;gt; Debug &amp;gt; Debugger Shell)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Mar 2013 06:58:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282647#M10465</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-03-22T06:58:15Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10.x how to expand several structures at once</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282648#M10466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Norm, was this helpful? Please keep us posted! :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards!&lt;/P&gt;&lt;P&gt;Monica&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2013 22:10:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282648#M10466</guid>
      <dc:creator>Monica</dc:creator>
      <dc:date>2013-04-03T22:10:34Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10.x how to expand several structures at once</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282649#M10467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Norm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Go to Project-&amp;gt;Properties-&amp;gt;C/C++ General-&amp;gt;Configure Workspace Settings (link at the right up window corner).&lt;/P&gt;&lt;P&gt;In the Preferences window-&amp;gt;C/C++-&amp;gt;Editor-&amp;gt;Folding. Check here all options that are you want to use.&lt;/P&gt;&lt;P&gt;May be this will help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;P&gt;Evgeni&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Apr 2013 06:16:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282649#M10467</guid>
      <dc:creator>evgenik</dc:creator>
      <dc:date>2013-04-05T06:16:08Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 10.x how to expand several structures at once</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282650#M10468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I took a quick look at how to use the debugger shell and I didn't see how a script would expand structures in the debugger GUI where the local variables are shown for the running program.&amp;nbsp; Are there examples of code that does something like this around?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2013 21:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Codewarrior-10-x-how-to-expand-several-structures-at-once/m-p/282650#M10468</guid>
      <dc:creator>nmay</dc:creator>
      <dc:date>2013-04-08T21:47:28Z</dc:date>
    </item>
  </channel>
</rss>