<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What are the basic and advanced compoents? in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-are-the-basic-and-advanced-compoents/m-p/280943#M10431</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you add a processor expert component to your project you can have 3 views.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Basic&lt;/P&gt;&lt;P&gt;- Anvaced&lt;/P&gt;&lt;P&gt;- Expert&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;You can set any module using the basic view. This view will let you configure basic module settings and leave all advanced settings as default. In advanced and expert view you can configure more specific settings of each module. For example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCG Module:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basic view: You will be able to set frequency and clock source.&lt;/P&gt;&lt;P&gt;Andvanced and profesional view: You will be able to specify if the clock will work in high gain or low power and set the internal capacitors values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PCR module:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basic view: You can determine a pin functionality (in case the pin has different options).&lt;/P&gt;&lt;P&gt;Adavnced and Profesional views: You can specify if it is open drain, slew rate and internal resistor value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Jun 2013 15:52:55 GMT</pubDate>
    <dc:creator>Carlos_Musich</dc:creator>
    <dc:date>2013-06-07T15:52:55Z</dc:date>
    <item>
      <title>What are the basic and advanced compoents?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-are-the-basic-and-advanced-compoents/m-p/280942#M10430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am new here. I read that Processor Expert has basic components and advanced components. I want to know what are they and what is different between them.&lt;/P&gt;&lt;P&gt;If I am using TWR-K60N512 board, do I need advanced components?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jun 2013 13:16:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-are-the-basic-and-advanced-compoents/m-p/280942#M10430</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2013-06-07T13:16:11Z</dc:date>
    </item>
    <item>
      <title>Re: What are the basic and advanced compoents?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-are-the-basic-and-advanced-compoents/m-p/280943#M10431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you add a processor expert component to your project you can have 3 views.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Basic&lt;/P&gt;&lt;P&gt;- Anvaced&lt;/P&gt;&lt;P&gt;- Expert&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;You can set any module using the basic view. This view will let you configure basic module settings and leave all advanced settings as default. In advanced and expert view you can configure more specific settings of each module. For example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCG Module:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basic view: You will be able to set frequency and clock source.&lt;/P&gt;&lt;P&gt;Andvanced and profesional view: You will be able to specify if the clock will work in high gain or low power and set the internal capacitors values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PCR module:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basic view: You can determine a pin functionality (in case the pin has different options).&lt;/P&gt;&lt;P&gt;Adavnced and Profesional views: You can specify if it is open drain, slew rate and internal resistor value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jun 2013 15:52:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-are-the-basic-and-advanced-compoents/m-p/280943#M10431</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2013-06-07T15:52:55Z</dc:date>
    </item>
    <item>
      <title>Re: What are the basic and advanced compoents?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-are-the-basic-and-advanced-compoents/m-p/280944#M10432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;Thank you for clarifying it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jun 2013 15:55:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-are-the-basic-and-advanced-compoents/m-p/280944#M10432</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2013-06-07T15:55:39Z</dc:date>
    </item>
    <item>
      <title>Re: What are the basic and advanced compoents?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-are-the-basic-and-advanced-compoents/m-p/280945#M10433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Daniel,&lt;/P&gt;&lt;P&gt;actually, this is not really true.&lt;/P&gt;&lt;P&gt;It is true that 'Basic', 'Advanced' and 'Expert' are view modes, and allow you to see more or less properties of a component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But 'Basic Components' and 'Advanced Components' are something different (and the terms have historical reasons):&lt;/P&gt;&lt;P&gt;- basic components are components like BitIO or InternalI2C or AsynchroSerial: drivers for the microcontroller peripherals.&lt;/P&gt;&lt;P&gt;- advanced components are software components on top of the basic components: e.g. Terminal, CAN software stack, etc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Historically, basic components were in the 'free of charge edition', while the 'advanced components' were available only in the paid editions. From CodeWarrior for MCU10.3 on (if I remember right), the 'advanced compents' are included in the 'free edition' too. So you should be able to use the 'Term' component, which is an Advanced Components.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So from this perspective, you should not need to care about if something is an advanced or basic component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jun 2013 16:47:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/What-are-the-basic-and-advanced-compoents/m-p/280945#M10433</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-06-07T16:47:06Z</dc:date>
    </item>
  </channel>
</rss>