<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Link ram and flash routines in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Link-ram-and-flash-routines/m-p/279063#M10380</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I need to run about 70KB of code faster. I think that running it in ram could increase the speed enough.&lt;/P&gt;&lt;P&gt;The software size is too big to run all&amp;nbsp; in ram so I need to use some code in flash and other in ram.&lt;/P&gt;&lt;P&gt;Some routines in ram have to call some routines in flash and vice versa.&lt;/P&gt;&lt;P&gt;Please is there a sample code that can load an executable library in ram at than calling routines (with codewarrior, micro k60)?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Alberto &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Apr 2013 10:29:31 GMT</pubDate>
    <dc:creator>albertomainoni</dc:creator>
    <dc:date>2013-04-22T10:29:31Z</dc:date>
    <item>
      <title>Link ram and flash routines</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Link-ram-and-flash-routines/m-p/279063#M10380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I need to run about 70KB of code faster. I think that running it in ram could increase the speed enough.&lt;/P&gt;&lt;P&gt;The software size is too big to run all&amp;nbsp; in ram so I need to use some code in flash and other in ram.&lt;/P&gt;&lt;P&gt;Some routines in ram have to call some routines in flash and vice versa.&lt;/P&gt;&lt;P&gt;Please is there a sample code that can load an executable library in ram at than calling routines (with codewarrior, micro k60)?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Alberto &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Apr 2013 10:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Link-ram-and-flash-routines/m-p/279063#M10380</guid>
      <dc:creator>albertomainoni</dc:creator>
      <dc:date>2013-04-22T10:29:31Z</dc:date>
    </item>
  </channel>
</rss>