<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: FreeMASTER with USB</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/FreeMASTER-with-USB/m-p/270550#M10148</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Markus,&lt;/P&gt;&lt;P&gt;FreeMASTER uses either serial or custom debug connection (JTAG/BDM/...) through a debug probe.&lt;/P&gt;&lt;P&gt;So that USB part is really USB CDC (USB over serial). So if you have intergrated the USB CDC code, this should go throug a virtual COM port on your PC.&lt;/P&gt;&lt;P&gt;So from the FreeMASTER perspective, it would look like a normal serial (COM) port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: there is no picture attached to your question.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Aug 2013 06:16:37 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2013-08-23T06:16:37Z</dc:date>
    <item>
      <title>FreeMASTER with USB</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/FreeMASTER-with-USB/m-p/270549#M10147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have successfully integrated the FreeMASTER serial driver to my application and can communicate between my Board (TowerSystem with the K60) and my host PC. I now want to migrate to use the USB connection for FreeMASTER. I see not much of a problem to adopt the USB drivers. However when I look into the communication tab of the FreeMASTER option dialog box I see nothing that belongs to USB (see picture) ? So which option for the communication do I have to setup ?&lt;/P&gt;&lt;P&gt;&lt;IMG style="width: 497px; height: 310.551px;" /&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2013 20:20:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/FreeMASTER-with-USB/m-p/270549#M10147</guid>
      <dc:creator>mkrug</dc:creator>
      <dc:date>2013-08-22T20:20:50Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMASTER with USB</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/FreeMASTER-with-USB/m-p/270550#M10148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Markus,&lt;/P&gt;&lt;P&gt;FreeMASTER uses either serial or custom debug connection (JTAG/BDM/...) through a debug probe.&lt;/P&gt;&lt;P&gt;So that USB part is really USB CDC (USB over serial). So if you have intergrated the USB CDC code, this should go throug a virtual COM port on your PC.&lt;/P&gt;&lt;P&gt;So from the FreeMASTER perspective, it would look like a normal serial (COM) port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: there is no picture attached to your question.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Aug 2013 06:16:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/FreeMASTER-with-USB/m-p/270550#M10148</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-08-23T06:16:37Z</dc:date>
    </item>
  </channel>
</rss>