<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Codewarrior 5.2 sometimes falls back to trial license in Software Licensing</title>
    <link>https://community.nxp.com/t5/Software-Licensing/Codewarrior-5-2-sometimes-falls-back-to-trial-license/m-p/519456#M994</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have a network (floating) license for Codewarrior Classic 5.2. After a few build's of my software, the linker error "L4025: This limited version allows only 65536 bytes of C code" appears and the link failed. When i wait a minute or two, and build again, it works as exprected.&lt;/P&gt;&lt;P&gt;We also use Codewarrior 10.6 with the same license model - without problems.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jun 2016 06:42:54 GMT</pubDate>
    <dc:creator>adrianteuscher</dc:creator>
    <dc:date>2016-06-13T06:42:54Z</dc:date>
    <item>
      <title>Codewarrior 5.2 sometimes falls back to trial license</title>
      <link>https://community.nxp.com/t5/Software-Licensing/Codewarrior-5-2-sometimes-falls-back-to-trial-license/m-p/519456#M994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have a network (floating) license for Codewarrior Classic 5.2. After a few build's of my software, the linker error "L4025: This limited version allows only 65536 bytes of C code" appears and the link failed. When i wait a minute or two, and build again, it works as exprected.&lt;/P&gt;&lt;P&gt;We also use Codewarrior 10.6 with the same license model - without problems.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jun 2016 06:42:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/Codewarrior-5-2-sometimes-falls-back-to-trial-license/m-p/519456#M994</guid>
      <dc:creator>adrianteuscher</dc:creator>
      <dc:date>2016-06-13T06:42:54Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior 5.2 sometimes falls back to trial license</title>
      <link>https://community.nxp.com/t5/Software-Licensing/Codewarrior-5-2-sometimes-falls-back-to-trial-license/m-p/519457#M995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;It will be good to see the log file located in LMTools.exe utility , also wondering if you are using comm&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Check the log file on the path specified &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36140i8195968BD505A891/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;If you are using multiple clients, sometime check in does not occur right away this might be a root cause. &lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jul 2016 20:13:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/Codewarrior-5-2-sometimes-falls-back-to-trial-license/m-p/519457#M995</guid>
      <dc:creator>TomasPaez</dc:creator>
      <dc:date>2016-07-08T20:13:48Z</dc:date>
    </item>
  </channel>
</rss>