<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Software Licensing中的主题 Re: FlexLM server Licensing</title>
    <link>https://community.nxp.com/t5/Software-Licensing/FlexLM-server-Licensing/m-p/254875#M361</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;just an additional info.&lt;/P&gt;&lt;P&gt;By default the feature(s) is(are) pre-reserved some times (5mn) for the same client/user.&lt;/P&gt;&lt;P&gt;The feature(s) can not be use immediately by another customer during this time, even if the CodeWarrior was closed on First client.&lt;/P&gt;&lt;P&gt;After 5mn the feature(s) will be available for other clients.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the rule is defined in Flexlm manual as lingering time.&lt;/P&gt;&lt;P&gt;For CodeWarrior the default value is 5mn.&lt;/P&gt;&lt;P&gt;The user can not reduce this time but can increase it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jan 2014 10:53:02 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2014-01-28T10:53:02Z</dc:date>
    <item>
      <title>FlexLM server Licensing</title>
      <link>https://community.nxp.com/t5/Software-Licensing/FlexLM-server-Licensing/m-p/254873#M359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;- Do I have to delete the enviremental variable which points to the license server in order to release the license copy for use by other colleagues or the normal closing of the application is sufficient for the release of the license number ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2013 12:13:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/FlexLM-server-Licensing/m-p/254873#M359</guid>
      <dc:creator>stankogradev</dc:creator>
      <dc:date>2013-12-11T12:13:55Z</dc:date>
    </item>
    <item>
      <title>Re: FlexLM server Licensing</title>
      <link>https://community.nxp.com/t5/Software-Licensing/FlexLM-server-Licensing/m-p/254874#M360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes, the normal closing of the application is sufficient for the release of the license number.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2013 02:21:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/FlexLM-server-Licensing/m-p/254874#M360</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2013-12-12T02:21:07Z</dc:date>
    </item>
    <item>
      <title>Re: FlexLM server Licensing</title>
      <link>https://community.nxp.com/t5/Software-Licensing/FlexLM-server-Licensing/m-p/254875#M361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;just an additional info.&lt;/P&gt;&lt;P&gt;By default the feature(s) is(are) pre-reserved some times (5mn) for the same client/user.&lt;/P&gt;&lt;P&gt;The feature(s) can not be use immediately by another customer during this time, even if the CodeWarrior was closed on First client.&lt;/P&gt;&lt;P&gt;After 5mn the feature(s) will be available for other clients.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the rule is defined in Flexlm manual as lingering time.&lt;/P&gt;&lt;P&gt;For CodeWarrior the default value is 5mn.&lt;/P&gt;&lt;P&gt;The user can not reduce this time but can increase it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2014 10:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/FlexLM-server-Licensing/m-p/254875#M361</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-01-28T10:53:02Z</dc:date>
    </item>
  </channel>
</rss>