<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Software LicensingのトピックRe: Evaluation license for &amp;quot;CodeWarrior for Microcontrollers v6.3&amp;quot; not working</title>
    <link>https://community.nxp.com/t5/Software-Licensing/Evaluation-license-for-quot-CodeWarrior-for-Microcontrollers-v6/m-p/1836773#M1859</link>
    <description>&lt;P&gt;Hello Jorge, I already gave the licenses files when you requested in Support Case 00604745&lt;/P&gt;</description>
    <pubDate>Wed, 27 Mar 2024 22:11:19 GMT</pubDate>
    <dc:creator>guix</dc:creator>
    <dc:date>2024-03-27T22:11:19Z</dc:date>
    <item>
      <title>Evaluation license for "CodeWarrior for Microcontrollers v6.3" not working</title>
      <link>https://community.nxp.com/t5/Software-Licensing/Evaluation-license-for-quot-CodeWarrior-for-Microcontrollers-v6/m-p/1829712#M1851</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am a hobbyist and a new user of Codewarrior IDE, I'm trying to repurpose an old device which uses a MC68HC908LJ12CFBE and a segmented LCD display, so I want to write a program for this microcontroller.&lt;/P&gt;&lt;P&gt;I have downloaded "&lt;SPAN&gt;CodeWarrior for Microcontrollers (RS08HC(S)08-ColdFire V1) v6.3.exe" but unfortunately it doesn't run on Windows 11 64bits, so instead I downloaded and installed an unofficial version of this software that I found here, thankfully :&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Installing-CodeWarrior-Classic-6-3-on-Windows-11-or-10-64-bit/m-p/1246050" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Installing-CodeWarrior-Classic-6-3-on-Windows-11-or-10-64-bit/m-p/1246050&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I have generated my license file, and put the content in "license.dat", I also manually ran "bin/regservers.bat" as I saw on a video in a similar question on this forum. I also tried to run the software with Administrator rights.&lt;/P&gt;&lt;P&gt;But still it's not working, almost nothing can be used in CodeWarrior or Processor Expert. Everything seem to be unlicensed and run in demo mode. For example, in Processor Expert, I try to add the 'Init_LCD" component, it says "Licensed component (Basic beans). You haven't any license to use it.", and when I click Generate Code, it will generate this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;void LCD1_Init(void)
{
/*
 #####  Here will be code if you have a full registered version  #####
*/
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-left" image-alt="cw.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/268782i6C5A1A9D1B56E624/image-size/medium?v=v2&amp;amp;px=400" role="button" title="cw.jpg" alt="cw.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;cw.jpg&lt;/span&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is an extract of my license.dat file, showing that I should be able to use the LCD component (right ?). I replaced some values with XXX, I don't know if that was important)&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;# License for ANY&lt;BR /&gt;INCREMENT PE_LCDHC08 metrowks 1.0 14-apr-2024 uncounted XXXXXXXXXXXX \&lt;BR /&gt;VENDOR_STRING="CodeWarrior for Microcontrollers - Professional \&lt;BR /&gt;Edition Evaluation / Updates" HOSTID=ANY ISSUER="NXP \&lt;BR /&gt;Semiconductor" ISSUED=16-mar-2024 ck=142 SN="FSL - XXXXXXX" \&lt;BR /&gt;TS_OK&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Can someone tell me what I am doing wrong ? Can it be because I am not using the official software ? If so, is there any solution to run the original software on Windows 11 64bits ?&lt;/P&gt;&lt;P&gt;Please help, I have already renewed my evaluation license once, because I'm stuck here since more than a month &lt;LI-EMOJI id="lia_disappointed-face" title=":disappointed_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Edit : Just to try, I've installed the official software on a VirtualBox running Windows XP SP3 32bits, I didn't even need to modify license.dat and everything seems to be unlocked and working as it should ! So it seems to be a problem with the unofficial software, sadly.&lt;/P&gt;</description>
      <pubDate>Sat, 16 Mar 2024 14:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/Evaluation-license-for-quot-CodeWarrior-for-Microcontrollers-v6/m-p/1829712#M1851</guid>
      <dc:creator>guix</dc:creator>
      <dc:date>2024-03-16T14:14:19Z</dc:date>
    </item>
    <item>
      <title>Re: Evaluation license for "CodeWarrior for Microcontrollers v6.3" not working</title>
      <link>https://community.nxp.com/t5/Software-Licensing/Evaluation-license-for-quot-CodeWarrior-for-Microcontrollers-v6/m-p/1836765#M1854</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Guillaume,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Can you share your license with me, it seams that youare trying to use some beans that are not free and need to be added to your evaluation.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Wed, 27 Mar 2024 21:49:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/Evaluation-license-for-quot-CodeWarrior-for-Microcontrollers-v6/m-p/1836765#M1854</guid>
      <dc:creator>jorge_plascencia</dc:creator>
      <dc:date>2024-03-27T21:49:33Z</dc:date>
    </item>
    <item>
      <title>Re: Evaluation license for "CodeWarrior for Microcontrollers v6.3" not working</title>
      <link>https://community.nxp.com/t5/Software-Licensing/Evaluation-license-for-quot-CodeWarrior-for-Microcontrollers-v6/m-p/1836773#M1859</link>
      <description>&lt;P&gt;Hello Jorge, I already gave the licenses files when you requested in Support Case 00604745&lt;/P&gt;</description>
      <pubDate>Wed, 27 Mar 2024 22:11:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/Evaluation-license-for-quot-CodeWarrior-for-Microcontrollers-v6/m-p/1836773#M1859</guid>
      <dc:creator>guix</dc:creator>
      <dc:date>2024-03-27T22:11:19Z</dc:date>
    </item>
  </channel>
</rss>