<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Software LicensingのトピックCW 10.3 license</title>
    <link>https://community.nxp.com/t5/Software-Licensing/CW-10-3-license/m-p/942511#M1725</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since many years, I used the CW10.3 with a buy license, with the P&amp;amp;E multilink universal.&lt;/P&gt;&lt;P&gt;With this, I use some Kinetis (with KDS without problem) and on HCS08 (MC13213) with CW v10.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I changed my computer by the beginning of this year.&lt;/P&gt;&lt;P&gt;Currently, I need do some rework on the old project using CW 10.3, P&amp;amp;E ML universal and MC13213.&lt;/P&gt;&lt;P&gt;But I have problem with codewarior 10.3 which is unable to upgrade the Pemicro firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pemicro support indicate to meCWv10.3 is not supported with new firmware.&lt;/P&gt;&lt;P&gt;Then I waiting her answer to get old firmwas which was compatible....&lt;/P&gt;&lt;P&gt;Or he advice to me to pass to CW v11.1...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I seen here CWv11.1 is evaluation version of 45day...&lt;/P&gt;&lt;P&gt;1) Is possible to move my v10.3 license to the v11.1?&lt;/P&gt;&lt;P&gt;2) Or could I retry here some P&amp;amp;E micro driver/firmware to make it work currently with the CW v10.3?...&lt;/P&gt;&lt;P&gt;3) It is easy to migrate CW10.3 project to CW v11.1?&lt;/P&gt;&lt;P&gt;4) May be can I use MCU expresso? (Is free of charge? Without licence? How port CW v10.3 project to MCUExpresso?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Arnaud&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Sep 2019 14:34:37 GMT</pubDate>
    <dc:creator>arnogir</dc:creator>
    <dc:date>2019-09-03T14:34:37Z</dc:date>
    <item>
      <title>CW 10.3 license</title>
      <link>https://community.nxp.com/t5/Software-Licensing/CW-10-3-license/m-p/942511#M1725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since many years, I used the CW10.3 with a buy license, with the P&amp;amp;E multilink universal.&lt;/P&gt;&lt;P&gt;With this, I use some Kinetis (with KDS without problem) and on HCS08 (MC13213) with CW v10.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I changed my computer by the beginning of this year.&lt;/P&gt;&lt;P&gt;Currently, I need do some rework on the old project using CW 10.3, P&amp;amp;E ML universal and MC13213.&lt;/P&gt;&lt;P&gt;But I have problem with codewarior 10.3 which is unable to upgrade the Pemicro firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pemicro support indicate to meCWv10.3 is not supported with new firmware.&lt;/P&gt;&lt;P&gt;Then I waiting her answer to get old firmwas which was compatible....&lt;/P&gt;&lt;P&gt;Or he advice to me to pass to CW v11.1...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I seen here CWv11.1 is evaluation version of 45day...&lt;/P&gt;&lt;P&gt;1) Is possible to move my v10.3 license to the v11.1?&lt;/P&gt;&lt;P&gt;2) Or could I retry here some P&amp;amp;E micro driver/firmware to make it work currently with the CW v10.3?...&lt;/P&gt;&lt;P&gt;3) It is easy to migrate CW10.3 project to CW v11.1?&lt;/P&gt;&lt;P&gt;4) May be can I use MCU expresso? (Is free of charge? Without licence? How port CW v10.3 project to MCUExpresso?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Arnaud&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2019 14:34:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/CW-10-3-license/m-p/942511#M1725</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2019-09-03T14:34:37Z</dc:date>
    </item>
    <item>
      <title>Re: CW 10.3 license</title>
      <link>https://community.nxp.com/t5/Software-Licensing/CW-10-3-license/m-p/942512#M1726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arnaud,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;But I have problem with codewarior 10.3 which is unable to upgrade the Pemicro firmware.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you share some screenshots of the exact error messages that you're getting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you're just having problems switching our Multilink firmware to the correct architecture (because you were using it with a different architecture before), you can use our PEMicro Multilink Universal Firmware Config utility.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.pemicro.com/downloads/download_file.cfm?download_id=346" title="http://www.pemicro.com/downloads/download_file.cfm?download_id=346"&gt;http://www.pemicro.com/downloads/download_file.cfm?download_id=346&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Johnny&lt;/P&gt;&lt;P&gt;PEmicro Support&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Sep 2019 16:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/CW-10-3-license/m-p/942512#M1726</guid>
      <dc:creator>johnny_pe</dc:creator>
      <dc:date>2019-09-10T16:39:32Z</dc:date>
    </item>
    <item>
      <title>Re: CW 10.3 license</title>
      <link>https://community.nxp.com/t5/Software-Licensing/CW-10-3-license/m-p/942513#M1727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I contacted the Pemicro support one week ago and provide to me the driver included into Cw11.1 to put into Cw10.3 installation path.&lt;/P&gt;&lt;P&gt;This work properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had tested with the PEMicro ML universale firmware config utility, this firmware work and flash the proble, but after taht, into codewarrior when I flash to the target, we went upgrade the firmware also and then generate an error..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2019 10:30:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/CW-10-3-license/m-p/942513#M1727</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2019-09-11T10:30:00Z</dc:date>
    </item>
  </channel>
</rss>