<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ARMv8 Codewarrior licensing in Software Licensing</title>
    <link>https://community.nxp.com/t5/Software-Licensing/ARMv8-Codewarrior-licensing/m-p/736747#M1278</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using Codewarrior for several processor platforms (PPC and ARM devices).&lt;/P&gt;&lt;P&gt;I use a floating license, generated for the following products :&lt;/P&gt;&lt;P&gt;&amp;nbsp;* 11.1&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;Specialist Level Features for License Files (DDR Validation, SerDes Validation, Packet Tool, Scenarios Tool)&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Specialist Level Features for License Files (DDR Validation, SerDes Validation, Scenarios Tool)&lt;BR /&gt;&amp;nbsp;* 10.4&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;CodeWarrior for Power Architecture - Professional Edition (Eclipse-Windows hosted)&lt;BR /&gt;&amp;nbsp;* 10.51&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; CodeWarrior for Power Architecture - Professional Edition (Eclipse-Windows hosted)&lt;BR /&gt;&amp;nbsp;* 11.2.3&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp; CodeWarrior for QorIQ LS Series ARMv8 ISA .&lt;BR /&gt;&amp;nbsp;* 11.2.0&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp; CodeWarrior for QorIQ LS Series ARMv8 ISA .&lt;BR /&gt;&amp;nbsp;* 11.1&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;CodeWarrior for QorIQ LS Series ARMv8 ISA .&lt;/P&gt;&lt;P&gt;CW for PPC architectures v10.4 and 10.5.1 are working fine, like CW4NET for ARM7.&lt;/P&gt;&lt;P&gt;But I have licensing issue with the CW4NET for ARM8 software. Here is the NXP license status for this application:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32029i5AB7C84B910F1854/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The result of the lmstat command ran on the client machine is attached to this post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; Is there specific licensing instructions for this software ?&lt;/P&gt;&lt;P&gt;=&amp;gt; Should I use another software version ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Dec 2017 14:52:49 GMT</pubDate>
    <dc:creator>xabiven</dc:creator>
    <dc:date>2017-12-21T14:52:49Z</dc:date>
    <item>
      <title>ARMv8 Codewarrior licensing</title>
      <link>https://community.nxp.com/t5/Software-Licensing/ARMv8-Codewarrior-licensing/m-p/736747#M1278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using Codewarrior for several processor platforms (PPC and ARM devices).&lt;/P&gt;&lt;P&gt;I use a floating license, generated for the following products :&lt;/P&gt;&lt;P&gt;&amp;nbsp;* 11.1&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;Specialist Level Features for License Files (DDR Validation, SerDes Validation, Packet Tool, Scenarios Tool)&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Specialist Level Features for License Files (DDR Validation, SerDes Validation, Scenarios Tool)&lt;BR /&gt;&amp;nbsp;* 10.4&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;CodeWarrior for Power Architecture - Professional Edition (Eclipse-Windows hosted)&lt;BR /&gt;&amp;nbsp;* 10.51&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; CodeWarrior for Power Architecture - Professional Edition (Eclipse-Windows hosted)&lt;BR /&gt;&amp;nbsp;* 11.2.3&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp; CodeWarrior for QorIQ LS Series ARMv8 ISA .&lt;BR /&gt;&amp;nbsp;* 11.2.0&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp; CodeWarrior for QorIQ LS Series ARMv8 ISA .&lt;BR /&gt;&amp;nbsp;* 11.1&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;CodeWarrior for QorIQ LS Series ARMv8 ISA .&lt;/P&gt;&lt;P&gt;CW for PPC architectures v10.4 and 10.5.1 are working fine, like CW4NET for ARM7.&lt;/P&gt;&lt;P&gt;But I have licensing issue with the CW4NET for ARM8 software. Here is the NXP license status for this application:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32029i5AB7C84B910F1854/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The result of the lmstat command ran on the client machine is attached to this post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; Is there specific licensing instructions for this software ?&lt;/P&gt;&lt;P&gt;=&amp;gt; Should I use another software version ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Dec 2017 14:52:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/ARMv8-Codewarrior-licensing/m-p/736747#M1278</guid>
      <dc:creator>xabiven</dc:creator>
      <dc:date>2017-12-21T14:52:49Z</dc:date>
    </item>
    <item>
      <title>Re: ARMv8 Codewarrior licensing</title>
      <link>https://community.nxp.com/t5/Software-Licensing/ARMv8-Codewarrior-licensing/m-p/736748#M1279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm answering myself to my question if it can help someone else in the future.&lt;/P&gt;&lt;P&gt;The problem is that it is required to copy the license file which is on the LM server in the installation directory of the client.&lt;/P&gt;&lt;P&gt;For me, the "license.dat" file must be present here : C:\Freescale\CW4NET_v2017.03\Common&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had the same behavior for the CW_PA_10.4, whereas the CW_PA_v10.5.1 can run with only the METROWKS_LICENSE_FILE variable set.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 13:41:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Software-Licensing/ARMv8-Codewarrior-licensing/m-p/736748#M1279</guid>
      <dc:creator>xabiven</dc:creator>
      <dc:date>2018-01-17T13:41:12Z</dc:date>
    </item>
  </channel>
</rss>