<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Codewarrior tap and script writing in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-and-script-writing/m-p/2358206#M9384</link>
    <description>&lt;P&gt;&lt;SPAN&gt;There are two ways to launch LA1224/VSPA in CW,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Debug Configuration UI&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Here you can set correct connection, then click 'Debug' to launchLA1224/VSPA&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. Debugger shell&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Here you can run tcl script to launch LA1224/vspa&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In folder Help/pdf there is a file "Targeting VSPA.pdf" in which the above settings are introduced in detail. Besides in folder Example there are sample projects showing the steps/settings&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 29 Apr 2026 04:15:57 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2026-04-29T04:15:57Z</dc:date>
    <item>
      <title>Codewarrior tap and script writing</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-and-script-writing/m-p/2357046#M9378</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I'm using CW_VSPA_v10.3.10. After successfully debugging my code, I don't know how to deploy it to the hardware with codewarrior tap. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The board I'm using is LA1224.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;I tried to write a script and load into ccs but failed, so are there any examples or instructions that can tell me how to&amp;nbsp;write a script?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Apr 2026 08:08:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-and-script-writing/m-p/2357046#M9378</guid>
      <dc:creator>tianzc</dc:creator>
      <dc:date>2026-04-28T08:08:52Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior tap and script writing</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-and-script-writing/m-p/2358206#M9384</link>
      <description>&lt;P&gt;&lt;SPAN&gt;There are two ways to launch LA1224/VSPA in CW,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Debug Configuration UI&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Here you can set correct connection, then click 'Debug' to launchLA1224/VSPA&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. Debugger shell&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Here you can run tcl script to launch LA1224/vspa&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In folder Help/pdf there is a file "Targeting VSPA.pdf" in which the above settings are introduced in detail. Besides in folder Example there are sample projects showing the steps/settings&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Apr 2026 04:15:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Codewarrior-tap-and-script-writing/m-p/2358206#M9384</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2026-04-29T04:15:57Z</dc:date>
    </item>
  </channel>
</rss>