<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Help with MCF5253 and USBDM-JMXX-CF in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Help-with-MCF5253-and-USBDM-JMXX-CF/m-p/2149536#M9326</link>
    <description>&lt;P&gt;Thank you so much !&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
    <pubDate>Sun, 10 Aug 2025 13:55:00 GMT</pubDate>
    <dc:creator>Yako66</dc:creator>
    <dc:date>2025-08-10T13:55:00Z</dc:date>
    <item>
      <title>Help with MCF5253 and USBDM-JMXX-CF</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Help-with-MCF5253-and-USBDM-JMXX-CF/m-p/2145665#M9324</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I'm new to embedded systems and would really appreciate any help or suggestions regarding a boot loop issue I'm experiencing with the MCF5253&amp;nbsp;&lt;/P&gt;&lt;P&gt;System Details:&lt;/P&gt;&lt;P&gt;&amp;nbsp;MCF5253&lt;/P&gt;&lt;P&gt;SDRAM :&amp;nbsp;MT48LC4M16A2&lt;/P&gt;&lt;P&gt;FLASH : M25P32&lt;/P&gt;&lt;P&gt;&lt;!-- StartFragment  --&gt;&lt;/P&gt;&lt;P&gt;To troubleshoot the boot loop, I purchased a USBDM-JMXX-CF interface to connect to the MCF5253 via BDM. My goal is to identify where the system is stalling during startup.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Tools &amp;amp; Versions:&lt;BR /&gt;- USBDM-JMXX-CF(software version 4.12)&lt;BR /&gt;- USBDM_4_12_1_340_Win.msi&lt;BR /&gt;- CodeWarrior 10.7&lt;/P&gt;&lt;P&gt;BDM connection pins:&lt;/P&gt;&lt;P&gt;-BKPT&lt;/P&gt;&lt;P&gt;-DSCLK&lt;/P&gt;&lt;P&gt;-DSI&lt;/P&gt;&lt;P&gt;-DSO&lt;/P&gt;&lt;P&gt;-RSTIO -&amp;gt;to rst pin of MCF5253&lt;/P&gt;&lt;P&gt;-PST0-4&lt;/P&gt;&lt;P&gt;-GND&amp;nbsp;&lt;/P&gt;&lt;P&gt;-VDD_BDM&lt;/P&gt;&lt;P&gt;&amp;nbsp;When I try to connect with CodeWarrior 10.7, the connection fails with the following error:&lt;/P&gt;&lt;P&gt;&lt;!-- EndFragment  --&gt;:&amp;nbsp;Error launching MCF5253_Console_RAM_USBDM&lt;BR /&gt;ColdFire GDI Protocol Adapter : Can't connect. Unknown or not supported device.&lt;/P&gt;&lt;P&gt;I also tested communication using the standalone USBDM application. Here’s the output from a memory dump attempt:&lt;/P&gt;&lt;P&gt;USBDM MEMORY DUMP :&lt;/P&gt;&lt;P&gt;&amp;nbsp;Creating Empty flash image...&lt;BR /&gt;Interface options: CFVx, , speed = 250&lt;BR /&gt;Using Memory space =&lt;BR /&gt;Reading memory-block[0x20000000, 0x20000010, 1]...&lt;BR /&gt;Done&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;!-- StartFragment  --&gt;&lt;/P&gt;&lt;P&gt;I'd appreciate any insights or suggestions, especially on the following points:&lt;/P&gt;&lt;P&gt;1. Has anyone successfully connected to an MCF5253 using a USBDM-JMXX-CF?&lt;BR /&gt;2. Is CodeWarrior 10.7 compatible with this setup, or are there known issues?&lt;BR /&gt;3. Are there specific configuration steps required to enable BDM communication?&lt;BR /&gt;4. Any general advice for debugging boot loops on ColdFire processors?&lt;/P&gt;&lt;P&gt;Thank you in advance for your help and support!&lt;/P&gt;&lt;P&gt;&lt;!-- EndFragment  --&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 02 Aug 2025 15:49:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Help-with-MCF5253-and-USBDM-JMXX-CF/m-p/2145665#M9324</guid>
      <dc:creator>Yako66</dc:creator>
      <dc:date>2025-08-02T15:49:34Z</dc:date>
    </item>
    <item>
      <title>Re: Help with MCF5253 and USBDM-JMXX-CF</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Help-with-MCF5253-and-USBDM-JMXX-CF/m-p/2147158#M9325</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Sorry for the later reply.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/development-software/codewarrior-development-tools/codewarrior-legacy/codewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-qorivva-56xx-rs08-s08-s12z-11-1:CW-MCU10" target="_self"&gt;CodeWarrior for MCUs (Eclipse IDE)&lt;/A&gt; supports OSBDM debugger tool.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Hui_Ma_0-1754442232113.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/351050i2EA8A0F1497F1F0D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Hui_Ma_0-1754442232113.png" alt="Hui_Ma_0-1754442232113.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Hui_Ma_0-1754442232113.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;There are two documents about OSBDM, please refer below links for details:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4331.pdf" target="_self"&gt;AN4331&lt;/A&gt;: Enabling OSBDM DLLs&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true" target="_self"&gt;OSBDM-JM60 user guide&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;You also could find OSBDM basic info from P&amp;amp;E website:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.pemicro.com/osbdm/osbdm_description.cfm" target="_blank"&gt;https://www.pemicro.com/osbdm/osbdm_description.cfm&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;While,&amp;nbsp;P&amp;amp;E has discontinued support for OSBDM.&lt;/P&gt;
&lt;P&gt;We recommend to use &lt;A href="https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180&amp;amp;productTab=5045" target="_self"&gt;P&amp;amp;E Multilink debug probes&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Thanks for the attention.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Aug 2025 01:13:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Help-with-MCF5253-and-USBDM-JMXX-CF/m-p/2147158#M9325</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2025-08-06T01:13:08Z</dc:date>
    </item>
    <item>
      <title>Re: Help with MCF5253 and USBDM-JMXX-CF</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Help-with-MCF5253-and-USBDM-JMXX-CF/m-p/2149536#M9326</link>
      <description>&lt;P&gt;Thank you so much !&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Sun, 10 Aug 2025 13:55:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Help-with-MCF5253-and-USBDM-JMXX-CF/m-p/2149536#M9326</guid>
      <dc:creator>Yako66</dc:creator>
      <dc:date>2025-08-10T13:55:00Z</dc:date>
    </item>
  </channel>
</rss>