<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Hardware communication issues with coldfire V1 MCF51JM128 in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Hardware-communication-issues-with-coldfire-V1-MCF51JM128/m-p/315762#M925</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like someone to please look at this code particularly the portserial files and interrupts to determine what&amp;nbsp; I'm doing wrong. I was finally able to build the code but unable to communicate to it. When I attempt to debug, it hangs up on an exception. The code is attached. Thanks&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337781"&gt;mb_6_6_2014.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 07 Jun 2014 13:08:44 GMT</pubDate>
    <dc:creator>yomioye2006</dc:creator>
    <dc:date>2014-06-07T13:08:44Z</dc:date>
    <item>
      <title>Hardware communication issues with coldfire V1 MCF51JM128</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Hardware-communication-issues-with-coldfire-V1-MCF51JM128/m-p/315762#M925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like someone to please look at this code particularly the portserial files and interrupts to determine what&amp;nbsp; I'm doing wrong. I was finally able to build the code but unable to communicate to it. When I attempt to debug, it hangs up on an exception. The code is attached. Thanks&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337781"&gt;mb_6_6_2014.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Jun 2014 13:08:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Hardware-communication-issues-with-coldfire-V1-MCF51JM128/m-p/315762#M925</guid>
      <dc:creator>yomioye2006</dc:creator>
      <dc:date>2014-06-07T13:08:44Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware communication issues with coldfire V1 MCF51JM128</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Hardware-communication-issues-with-coldfire-V1-MCF51JM128/m-p/315763#M926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi, please accept my apology for the time it has taken us to get back to you on this issue.&lt;/P&gt;&lt;P&gt;I've tried your project on my side, it seems works (I did not connect the target MCF51JM128 board to a serial port).&lt;/P&gt;&lt;P&gt;and I did not see the problem hanging up on an exception.&lt;/P&gt;&lt;P&gt;if your problem still remains, then, could you please let me know the steps to reproduce your problem.&lt;/P&gt;&lt;P&gt;it would be better if you could upload an image showing the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jun 2014 07:36:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Hardware-communication-issues-with-coldfire-V1-MCF51JM128/m-p/315763#M926</guid>
      <dc:creator>Rick_Li</dc:creator>
      <dc:date>2014-06-13T07:36:33Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware communication issues with coldfire V1 MCF51JM128</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Hardware-communication-issues-with-coldfire-V1-MCF51JM128/m-p/315764#M927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yong,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm unable to generate any responses from the Modbus poll I'm using. It doesn't bseem to talk back or even recognise the communication. When i debug I hang up at this exception pasted below at line link a6, #0. what cpould be the issue? I'm using the latest codearrior 10.6 and debugger. Can you please look at my hardware settings? Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; derivative_interrupt(stackFrameVector);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;asm&amp;nbsp; __declspec(register_abi) void asm_exception_handler(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; link&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; a6,#0 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; lea&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -20(sp), sp&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; movem.l d0-d2/a0-a1, (sp)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; lea&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 24(sp),a0&amp;nbsp;&amp;nbsp; // A0 point to exception stack frame on the stack &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; jsr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mcf_exception_handler&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; movem.l (sp), d0-d2/a0-a1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; lea&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 20(sp), sp&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; unlk a6&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; rte&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;typedef void (* vectorTableEntryType)(void);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jun 2014 13:20:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Hardware-communication-issues-with-coldfire-V1-MCF51JM128/m-p/315764#M927</guid>
      <dc:creator>yomioye2006</dc:creator>
      <dc:date>2014-06-13T13:20:44Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware communication issues with coldfire V1 MCF51JM128</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Hardware-communication-issues-with-coldfire-V1-MCF51JM128/m-p/315765#M928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yomi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Very sorry for the delay.&lt;/P&gt;&lt;P&gt;My colleague Li has logged the problem under the SR 1-1617271101.&lt;/P&gt;&lt;P&gt;Li will investigate the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't have experience with Modbus.&lt;/P&gt;&lt;P&gt;The asm_exception_handler() is used when the ISR is not defined in the application.&lt;/P&gt;&lt;P&gt;This is the default function used by ISR.&lt;/P&gt;&lt;P&gt;So if your application fall inside this function, this means an ISR which is not defined in your application is generated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jun 2014 13:38:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Hardware-communication-issues-with-coldfire-V1-MCF51JM128/m-p/315765#M928</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2014-06-17T13:38:23Z</dc:date>
    </item>
  </channel>
</rss>