<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Debugging U-boot from nor Flash using T2081 processor in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Debugging-U-boot-from-nor-Flash-using-T2081-processor/m-p/1941677#M9168</link>
    <description>&lt;P&gt;I am trying to debug the U-boot from the NOR-Flash location . I am using 128MB&amp;nbsp; NOR Flash.&lt;/P&gt;&lt;P&gt;I have flashed the U-boot.bin in the address 0xEFF40000 according to 128M NOR flash memory map.&lt;/P&gt;&lt;P&gt;In document No. AN4876.pdf mentioned the steps for U-boot debugging for P1010.&lt;/P&gt;&lt;P&gt;I have followed the steps for T2081 but I can't see the source code for debugging.&lt;/P&gt;&lt;P&gt;After giving the path also it not entering into code.&lt;/P&gt;&lt;P&gt;So, currently we are checking in the Disassembly side , there we are starting from 0xEFFFFFFC and running step by step.&lt;/P&gt;&lt;P&gt;We were comparing the assembly code with start.S. While allocating Initial RAM in data cache&amp;nbsp; it is switches to the Instruction TLB error at 0xEFF40960 according with system.map file.&lt;/P&gt;&lt;P&gt;Can you give the solution for debugging the U-boot&amp;nbsp; from NOR-flash for T2081 processor in CodeWarrior?&lt;/P&gt;</description>
    <pubDate>Wed, 28 Aug 2024 02:21:28 GMT</pubDate>
    <dc:creator>Vimalprasad</dc:creator>
    <dc:date>2024-08-28T02:21:28Z</dc:date>
    <item>
      <title>Debugging U-boot from nor Flash using T2081 processor</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Debugging-U-boot-from-nor-Flash-using-T2081-processor/m-p/1941677#M9168</link>
      <description>&lt;P&gt;I am trying to debug the U-boot from the NOR-Flash location . I am using 128MB&amp;nbsp; NOR Flash.&lt;/P&gt;&lt;P&gt;I have flashed the U-boot.bin in the address 0xEFF40000 according to 128M NOR flash memory map.&lt;/P&gt;&lt;P&gt;In document No. AN4876.pdf mentioned the steps for U-boot debugging for P1010.&lt;/P&gt;&lt;P&gt;I have followed the steps for T2081 but I can't see the source code for debugging.&lt;/P&gt;&lt;P&gt;After giving the path also it not entering into code.&lt;/P&gt;&lt;P&gt;So, currently we are checking in the Disassembly side , there we are starting from 0xEFFFFFFC and running step by step.&lt;/P&gt;&lt;P&gt;We were comparing the assembly code with start.S. While allocating Initial RAM in data cache&amp;nbsp; it is switches to the Instruction TLB error at 0xEFF40960 according with system.map file.&lt;/P&gt;&lt;P&gt;Can you give the solution for debugging the U-boot&amp;nbsp; from NOR-flash for T2081 processor in CodeWarrior?&lt;/P&gt;</description>
      <pubDate>Wed, 28 Aug 2024 02:21:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Debugging-U-boot-from-nor-Flash-using-T2081-processor/m-p/1941677#M9168</guid>
      <dc:creator>Vimalprasad</dc:creator>
      <dc:date>2024-08-28T02:21:28Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging U-boot from nor Flash using T2081 processor</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Debugging-U-boot-from-nor-Flash-using-T2081-processor/m-p/1945359#M9169</link>
      <description>&lt;P&gt;In the application note&amp;nbsp;AN4876.pdf, please refer to section "5.2.2. Stage 1 – Debug NOR for AS0", Can you see the prompt information to ask for the source file marked in red?&lt;/P&gt;
&lt;P&gt;If yes, please click "Locate File" to specify the path of the source code.&lt;/P&gt;
&lt;P&gt;Please make sure the u-boot image running the target board is the latest and built from your current u-boot build environment.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Sep 2024 09:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Debugging-U-boot-from-nor-Flash-using-T2081-processor/m-p/1945359#M9169</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-09-02T09:22:37Z</dc:date>
    </item>
  </channel>
</rss>