<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: Linker error in Coldfire v2, CodeWarrior 7.1 to 7.2 conversion</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Linker-error-in-Coldfire-v2-CodeWarrior-7-1-to-7-2-conversion/m-p/1941636#M9167</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Due to&amp;nbsp;&lt;SPAN&gt;MCF520x_CWexample.zip related projects could build with CodeWarrior V7.2, could you compare related project build and linker configuration vs. your project.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The project linker files also need be compared if there existing any big difference.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Wish it helps.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 28 Aug 2024 00:55:44 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2024-08-28T00:55:44Z</dc:date>
    <item>
      <title>Linker error in Coldfire v2, CodeWarrior 7.1 to 7.2 conversion</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Linker-error-in-Coldfire-v2-CodeWarrior-7-1-to-7-2-conversion/m-p/1938669#M9164</link>
      <description>&lt;P&gt;I'm getting a:&lt;/P&gt;&lt;P&gt;"Error : Undefined "dtor_call(void*,void*,long)",&amp;nbsp;Referenced from "@ex@_dtor_call(void*,void*,long)" in&lt;/P&gt;&lt;P&gt;error after converting code originally developed in CodeWarrior 7.1 to CodeWarrior 7.2. I've followed the instructions in NXP technical note 268 (and video) and fixed other new errors after compiling/linking with 7.2, this is the only error I haven't resolved.&lt;/P&gt;&lt;P&gt;-------------------------&lt;/P&gt;&lt;P&gt;Original 7.1 Settings:&lt;/P&gt;&lt;P&gt;iNSIGHT4 Settings/Code Generation/ColdFire Processor&lt;BR /&gt;Target Family: 5207_8 CPU: 5207&lt;/P&gt;&lt;P&gt;Libs:&lt;BR /&gt;fp_coldfire.a&lt;BR /&gt;C_4i_CF_RegABI_MSL.a&lt;BR /&gt;C_4i_CF_RegABI_Runtime.a&lt;/P&gt;&lt;P&gt;-------------------------&lt;/P&gt;&lt;P&gt;CodeWarrior 7.2 changed Settings:&lt;/P&gt;&lt;P&gt;iNSIGHT4 Settings/Linker/Librarian&lt;BR /&gt;Control libraries is checked&lt;BR /&gt;Library model: c9x&lt;/P&gt;&lt;P&gt;-------------------------&lt;/P&gt;&lt;P&gt;The code is C and assembler. I'm not aware of any C++ code.&lt;/P&gt;&lt;P&gt;Any ideas how to eliminate the error? Are there other Settings that could cause this error?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Aug 2024 18:51:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Linker-error-in-Coldfire-v2-CodeWarrior-7-1-to-7-2-conversion/m-p/1938669#M9164</guid>
      <dc:creator>ken67</dc:creator>
      <dc:date>2024-08-22T18:51:39Z</dc:date>
    </item>
    <item>
      <title>Re: Linker error in Coldfire v2, CodeWarrior 7.1 to 7.2 conversion</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Linker-error-in-Coldfire-v2-CodeWarrior-7-1-to-7-2-conversion/m-p/1939974#M9165</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The &lt;A href="https://www.nxp.com/docs/en/application-note/TN268.pdf" target="_self"&gt;TN268&lt;/A&gt; (Converting Projects to CodeWarrior ColdFire V7.2) has below description:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Hui_Ma_0-1724653059634.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/295160i3B9184A3E1E2BB55/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Hui_Ma_0-1724653059634.png" alt="Hui_Ma_0-1724653059634.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Hui_Ma_0-1724653059634.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please try to select the library mode to "ewl".&lt;/P&gt;
&lt;P&gt;BTW: Please use attached CodeWarrior for MCF5208 projects do a test if meet the same linker error.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Mon, 26 Aug 2024 06:21:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Linker-error-in-Coldfire-v2-CodeWarrior-7-1-to-7-2-conversion/m-p/1939974#M9165</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2024-08-26T06:21:07Z</dc:date>
    </item>
    <item>
      <title>Re: Linker error in Coldfire v2, CodeWarrior 7.1 to 7.2 conversion</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Linker-error-in-Coldfire-v2-CodeWarrior-7-1-to-7-2-conversion/m-p/1941473#M9166</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The projects in&amp;nbsp;MCF520x_CWexample.zip don't generate the same linker error.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Using the "ewl" library mode generates the following errors (in&amp;nbsp;2408271052EwlLibraryErrors.txt file):&lt;/P&gt;&lt;P&gt;------------------------&lt;/P&gt;&lt;P&gt;Link Error : Undefined : "__strtoull"&lt;BR /&gt;Referenced from "__sformatterLL" in&lt;/P&gt;&lt;P&gt;Link Error : Undefined : "__strtoull"&lt;BR /&gt;Referenced from "__sformatter_FPLL" in&lt;/P&gt;&lt;P&gt;Link Error : Undefined : "__strtoull"&lt;BR /&gt;Referenced from "__sformatter_sLL" in&lt;/P&gt;&lt;P&gt;Link Error : Undefined : "__strtoull"&lt;BR /&gt;Referenced from "__sformatter_s_FPLL" in&lt;/P&gt;&lt;P&gt;Error : Undefined : "dtor_call(void*,void*,long)"&lt;BR /&gt;Referenced from "@ex@_dtor_call(void*,void*,long)" in&lt;/P&gt;&lt;P&gt;Link Error : Undefined : "strtof"&lt;BR /&gt;Referenced from "nanf" in&lt;/P&gt;&lt;P&gt;Link failed.&lt;/P&gt;&lt;P&gt;------------------------&lt;/P&gt;&lt;P&gt;Using the "c9x" library mode only generates the "Error : Undefined : "dtor_call(void*,void*,long)",&amp;nbsp;Referenced from "@ex@_dtor_call(void*,void*,long)" in" error (2408271054c9xLibraryErrors.txt). Same thing when&amp;nbsp;specifying the&amp;nbsp;C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\ColdFire_Support\ewl\lib\v2\libc99.a library in the Libs folder while in "ewl" library mode.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Aug 2024 18:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Linker-error-in-Coldfire-v2-CodeWarrior-7-1-to-7-2-conversion/m-p/1941473#M9166</guid>
      <dc:creator>ken67</dc:creator>
      <dc:date>2024-08-27T18:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: Linker error in Coldfire v2, CodeWarrior 7.1 to 7.2 conversion</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Linker-error-in-Coldfire-v2-CodeWarrior-7-1-to-7-2-conversion/m-p/1941636#M9167</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Due to&amp;nbsp;&lt;SPAN&gt;MCF520x_CWexample.zip related projects could build with CodeWarrior V7.2, could you compare related project build and linker configuration vs. your project.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The project linker files also need be compared if there existing any big difference.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Wish it helps.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Aug 2024 00:55:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Linker-error-in-Coldfire-v2-CodeWarrior-7-1-to-7-2-conversion/m-p/1941636#M9167</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2024-08-28T00:55:44Z</dc:date>
    </item>
  </channel>
</rss>