<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KIT MPXY8300A in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/KIT-MPXY8300A/m-p/314255#M912</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using the KIT MPXY8300A but I have many problems with the code.&lt;/P&gt;&lt;P&gt;There is an example in the MPXY8300 firmware user's manual but it doesn't work.&lt;/P&gt;&lt;P&gt;When I put it in CodeWarrior the program doesn't recognize the functions and subroutines ready for this kit as for example: &lt;/P&gt;&lt;P&gt;UINT8_MPXY8300_READ_COMP_ACCEL_X (UINT16 * Data, UINT16 TRaw, UINT8 Avg, UINT8 FilterSelect)&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;The code includes this libriary; "reims_firm_io_ES2.h" but I haven't it and I think the subroutines are implemented in this file.&lt;/P&gt;&lt;P&gt;Who know what I have to do or where can I find this library?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Jun 2014 12:03:52 GMT</pubDate>
    <dc:creator>riccardocescato</dc:creator>
    <dc:date>2014-06-04T12:03:52Z</dc:date>
    <item>
      <title>KIT MPXY8300A</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/KIT-MPXY8300A/m-p/314255#M912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using the KIT MPXY8300A but I have many problems with the code.&lt;/P&gt;&lt;P&gt;There is an example in the MPXY8300 firmware user's manual but it doesn't work.&lt;/P&gt;&lt;P&gt;When I put it in CodeWarrior the program doesn't recognize the functions and subroutines ready for this kit as for example: &lt;/P&gt;&lt;P&gt;UINT8_MPXY8300_READ_COMP_ACCEL_X (UINT16 * Data, UINT16 TRaw, UINT8 Avg, UINT8 FilterSelect)&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;The code includes this libriary; "reims_firm_io_ES2.h" but I haven't it and I think the subroutines are implemented in this file.&lt;/P&gt;&lt;P&gt;Who know what I have to do or where can I find this library?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jun 2014 12:03:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/KIT-MPXY8300A/m-p/314255#M912</guid>
      <dc:creator>riccardocescato</dc:creator>
      <dc:date>2014-06-04T12:03:52Z</dc:date>
    </item>
    <item>
      <title>Re: KIT MPXY8300A</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/KIT-MPXY8300A/m-p/314256#M913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi riccardo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i think attached project should include the file that you need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=====================================================&lt;/P&gt;&lt;P&gt;this answer is for you. if it helps, please click on "correct answer " button. thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jennie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 07:51:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/KIT-MPXY8300A/m-p/314256#M913</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-06-05T07:51:33Z</dc:date>
    </item>
    <item>
      <title>Re: KIT MPXY8300A</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/KIT-MPXY8300A/m-p/314257#M914</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks very much!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Only as confirmation, how can I create an empty project which those files?&lt;/P&gt;&lt;P&gt;I'm using CodeWarrior 10.6 and when I select a Bareboard Project for MPXY 8300 family I can't find such files.&lt;/P&gt;&lt;P&gt;Or better, how can I create I new project from your project? bucause if I create a new project from existing code it uses only the files in the Source directory and so there are problems with the "hidef.h" library.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;P&gt;RC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 17:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/KIT-MPXY8300A/m-p/314257#M914</guid>
      <dc:creator>riccardocescato</dc:creator>
      <dc:date>2014-06-09T17:04:07Z</dc:date>
    </item>
    <item>
      <title>Re: KIT MPXY8300A</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/KIT-MPXY8300A/m-p/314258#M915</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;please check thread:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/325054"&gt;KIT MPXY8300A&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 07:50:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/KIT-MPXY8300A/m-p/314258#M915</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-06-11T07:50:36Z</dc:date>
    </item>
  </channel>
</rss>