<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: CCSProtocolPlugin : Invalid parameter</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCSProtocolPlugin-Invalid-parameter/m-p/1679097#M8991</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;There is a document about &lt;A href="https://www.nxp.com.cn/docs/en/user-guide/USBTAPUG.pdf" target="_self"&gt;CodeWarrior USB TAP user guide&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;ColdFire product MCF52xx is using BDM interface, more detailed info please check appendix C.&lt;/P&gt;
&lt;P&gt;Thanks for the attention.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
    <pubDate>Fri, 30 Jun 2023 01:04:01 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2023-06-30T01:04:01Z</dc:date>
    <item>
      <title>CCSProtocolPlugin : Invalid parameter</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCSProtocolPlugin-Invalid-parameter/m-p/1677216#M8990</link>
      <description>&lt;P&gt;I am running CodeWarrior Development Studio V11.1&lt;/P&gt;&lt;P&gt;I am attempting to connect to an MCF52**.&lt;/P&gt;&lt;P&gt;I have a CodeWarrior TAP. (I do not believe this is the USB version although it does have a USB and ethernet port).&lt;/P&gt;&lt;P&gt;Currently I am connected via USB.&lt;/P&gt;&lt;P&gt;When creating a project I select&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Freescale USB TAP&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;In the Debug Configuration I have the session type selected as "Connect". Within the Connection I have a USB TAP with CCS Server set to "Automatic Launch". I have disabled all Initialization and Memory options such as Execute reset and Initialize target (I do not want to alter what is running on my system I just want to connect to it).&lt;/P&gt;&lt;P&gt;My system does not have a standard 16pin JTAG port for the CodeWarrior TAP so I have manually wired the signals. Specifically I have wired TDO, TDI, TRST, TGT PWR, TCK, TMS, and GND. I have not wired SRST or HRST.&lt;/P&gt;&lt;P&gt;On my TAP I see the Tx/Rx light blinking green and the Run/Pause light Red.&lt;/P&gt;&lt;P&gt;At this point I ask CodeWarrior to debug my device using the configs I have described above. In progress I see "Configuring CC" then it fails with&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Error launching &amp;lt;project_name&amp;gt; CCSProtocolPlugin : Invalid parameter&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I am trying to understand if this is an issue because my setup is incorrectly wired or if my TAP is improperly being used/configured. Right now I only have the device connected via USB to my computer. In device manager all I can find is the COM Port using default Windows drivers so I think that may be an issue but I am not sure. I tried connecting via ethernet but my companies VPN configs are giving me trouble there so I was hoping to just use USB if possible.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Any suggestion on what is wrong with my setup would be incredibly appreciated.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jun 2023 19:04:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCSProtocolPlugin-Invalid-parameter/m-p/1677216#M8990</guid>
      <dc:creator>PC_user1</dc:creator>
      <dc:date>2023-06-27T19:04:06Z</dc:date>
    </item>
    <item>
      <title>Re: CCSProtocolPlugin : Invalid parameter</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCSProtocolPlugin-Invalid-parameter/m-p/1679097#M8991</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;There is a document about &lt;A href="https://www.nxp.com.cn/docs/en/user-guide/USBTAPUG.pdf" target="_self"&gt;CodeWarrior USB TAP user guide&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;ColdFire product MCF52xx is using BDM interface, more detailed info please check appendix C.&lt;/P&gt;
&lt;P&gt;Thanks for the attention.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jun 2023 01:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/CCSProtocolPlugin-Invalid-parameter/m-p/1679097#M8991</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2023-06-30T01:04:01Z</dc:date>
    </item>
  </channel>
</rss>