<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックLS1046A Development on the LS1046ARDB using CodeWarrior</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-Development-on-the-LS1046ARDB-using-CodeWarrior/m-p/1505790#M8845</link>
    <description>&lt;P&gt;Using Codewarrior, I am able to build a QorIQ Configuration Project for the PBL, and upload the RCW from the development kit.&amp;nbsp; Now I modify this RCW to disable the SerDes (or something), then compile the project, which generates a bin file in the "Generated_Code" directory.&amp;nbsp; If I use this file and update flash with it, it's endianness is wrong the next time I read it.&amp;nbsp; Is there an automated way from within CodeWarrior to fix this, or is it something we do manually.&lt;/P&gt;&lt;P&gt;I notice there is a utility in the LSDK when building this stuff from the command line.&lt;/P&gt;&lt;P&gt;Any pointers helpful.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Fri, 12 Aug 2022 22:21:12 GMT</pubDate>
    <dc:creator>Daves_Garage</dc:creator>
    <dc:date>2022-08-12T22:21:12Z</dc:date>
    <item>
      <title>LS1046A Development on the LS1046ARDB using CodeWarrior</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-Development-on-the-LS1046ARDB-using-CodeWarrior/m-p/1505790#M8845</link>
      <description>&lt;P&gt;Using Codewarrior, I am able to build a QorIQ Configuration Project for the PBL, and upload the RCW from the development kit.&amp;nbsp; Now I modify this RCW to disable the SerDes (or something), then compile the project, which generates a bin file in the "Generated_Code" directory.&amp;nbsp; If I use this file and update flash with it, it's endianness is wrong the next time I read it.&amp;nbsp; Is there an automated way from within CodeWarrior to fix this, or is it something we do manually.&lt;/P&gt;&lt;P&gt;I notice there is a utility in the LSDK when building this stuff from the command line.&lt;/P&gt;&lt;P&gt;Any pointers helpful.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 12 Aug 2022 22:21:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-Development-on-the-LS1046ARDB-using-CodeWarrior/m-p/1505790#M8845</guid>
      <dc:creator>Daves_Garage</dc:creator>
      <dc:date>2022-08-12T22:21:12Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A Development on the LS1046ARDB using CodeWarrior</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-Development-on-the-LS1046ARDB-using-CodeWarrior/m-p/1519889#M8852</link>
      <description>&lt;P&gt;You could use rcw package provided in LSDK.&lt;/P&gt;
&lt;P&gt;$ git clone &lt;A href="https://source.codeaurora.org/external/qoriq/qoriq-components/rcw.git" target="_blank"&gt;https://source.codeaurora.org/external/qoriq/qoriq-components/rcw.git&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;$&amp;nbsp;git checkout -b LSDK-21.08 LSDK-21.08&lt;/P&gt;
&lt;P&gt;$ cd rcw/ls1028ardb&lt;/P&gt;
&lt;P&gt;$ ../rcw.py -i R_SQPP_0x85bb/rcw_1500_gpu600.rcw -o R_SQPP_0x85bb/rcw_1500_gpu600.bin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Sep 2022 09:03:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-Development-on-the-LS1046ARDB-using-CodeWarrior/m-p/1519889#M8852</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-09-09T09:03:55Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A Development on the LS1046ARDB using CodeWarrior</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-Development-on-the-LS1046ARDB-using-CodeWarrior/m-p/1520019#M8853</link>
      <description>&lt;P&gt;Yes.&amp;nbsp; This was exactly pointed out in my question above.&amp;nbsp; "I notice there is a utility in the LSDK when building this stuff from the command line."&lt;/P&gt;&lt;P&gt;I am aware of the python script for building the rcw, and generating the bin file.&amp;nbsp; My question is specifically about programming the RCW from within the CodeWarrior software.&amp;nbsp; Using the flash utility and flashing the bin file generated from CodeWarrior doesn't account for the big-endian ordering.&amp;nbsp; The question I need answered is:&amp;nbsp; Is there a method or process within CodeWarrior for doing this?&lt;/P&gt;</description>
      <pubDate>Fri, 09 Sep 2022 13:40:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-Development-on-the-LS1046ARDB-using-CodeWarrior/m-p/1520019#M8853</guid>
      <dc:creator>Daves_Garage</dc:creator>
      <dc:date>2022-09-09T13:40:30Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A Development on the LS1046ARDB using CodeWarrior</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-Development-on-the-LS1046ARDB-using-CodeWarrior/m-p/1524629#M8863</link>
      <description>&lt;P&gt;No method in CodeWarrior to do this.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Sep 2022 03:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-Development-on-the-LS1046ARDB-using-CodeWarrior/m-p/1524629#M8863</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-09-20T03:44:39Z</dc:date>
    </item>
  </channel>
</rss>