<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development Toolsのトピックcopy code from target</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/copy-code-from-target/m-p/1449371#M8762</link>
    <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi to all:&lt;/P&gt;&lt;P&gt;I'm programming a noise cancellation algorithm on the 9s12C32 processor using Code Warrior v5.5.1272 with the True-Time Simulator and Debugger, V6.1&lt;/P&gt;&lt;P&gt;I started the project a few years ago, got Prototype #1 up and running, then had to set it aside for four years due to my wife's illness.&lt;/P&gt;&lt;P&gt;Now I am working with Prototype #2.&amp;nbsp; I programmed it with the most recent version of my algorithm.&lt;/P&gt;&lt;P&gt;I have both prototypes running side by side on my test bench, using the same input signal, but the output from Prototype #1 is a little cleaner.&lt;/P&gt;&lt;P&gt;Is there a way to read or copy the code in Prototype #1?&amp;nbsp; It's unsecured.&lt;/P&gt;&lt;P&gt;Would I be able to make sense of it so I can update my source code?&amp;nbsp; In the "code" column is the number 620, so I guess it uses 620 bytes?&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Tue, 26 Apr 2022 17:50:48 GMT</pubDate>
    <dc:creator>JohnnyP</dc:creator>
    <dc:date>2022-04-26T17:50:48Z</dc:date>
    <item>
      <title>copy code from target</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/copy-code-from-target/m-p/1449371#M8762</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi to all:&lt;/P&gt;&lt;P&gt;I'm programming a noise cancellation algorithm on the 9s12C32 processor using Code Warrior v5.5.1272 with the True-Time Simulator and Debugger, V6.1&lt;/P&gt;&lt;P&gt;I started the project a few years ago, got Prototype #1 up and running, then had to set it aside for four years due to my wife's illness.&lt;/P&gt;&lt;P&gt;Now I am working with Prototype #2.&amp;nbsp; I programmed it with the most recent version of my algorithm.&lt;/P&gt;&lt;P&gt;I have both prototypes running side by side on my test bench, using the same input signal, but the output from Prototype #1 is a little cleaner.&lt;/P&gt;&lt;P&gt;Is there a way to read or copy the code in Prototype #1?&amp;nbsp; It's unsecured.&lt;/P&gt;&lt;P&gt;Would I be able to make sense of it so I can update my source code?&amp;nbsp; In the "code" column is the number 620, so I guess it uses 620 bytes?&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 26 Apr 2022 17:50:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/copy-code-from-target/m-p/1449371#M8762</guid>
      <dc:creator>JohnnyP</dc:creator>
      <dc:date>2022-04-26T17:50:48Z</dc:date>
    </item>
    <item>
      <title>Re: copy code from target</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/copy-code-from-target/m-p/1449847#M8763</link>
      <description>&lt;P&gt;Please see answer in this thread&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Copy-code-from-my-target/td-p/1449145" target="_blank"&gt;https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Copy-code-from-my-target/td-p/1449145&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Apr 2022 10:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/copy-code-from-target/m-p/1449847#M8763</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-04-27T10:25:19Z</dc:date>
    </item>
  </channel>
</rss>