<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: LS1046A-FRWY system hangs when CodeWarrior connects</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-FRWY-system-hangs-when-CodeWarrior-connects/m-p/1448274#M8760</link>
    <description>&lt;P&gt;Do you want to use CodeWarrior to connect to the target board to do Linux Kernel debugging?&lt;/P&gt;
&lt;P&gt;If yes, please refer to CodeWarrior configuration in section 3 in this document.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-boot-and-Linux-Kernel-and/ta-p/1114872" target="_blank"&gt;https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-boot-and-Linux-Kernel-and/ta-p/1114872&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 25 Apr 2022 05:27:07 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-04-25T05:27:07Z</dc:date>
    <item>
      <title>LS1046A-FRWY system hangs when CodeWarrior connects</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-FRWY-system-hangs-when-CodeWarrior-connects/m-p/1448119#M8759</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm running the LS1046A Yocto SDK (5.4.3+g134788b16485). It boots fine and mounts its rootfs from the SD Card. When CodeWarrior connects, I get the following message on the terminal and then the terminal hangs.&lt;/P&gt;&lt;P&gt;"EXT4-fs (mmcblk0p3): re-mounted. Opts: (null)"&lt;/P&gt;&lt;P&gt;If I run rootfs from a RAM disk, the system seems to run fine with CodeWarrior.&lt;/P&gt;&lt;P&gt;I'm looking for suggestions on how to resolve this problem. Thank you.&lt;/P&gt;</description>
      <pubDate>Sun, 24 Apr 2022 04:19:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-FRWY-system-hangs-when-CodeWarrior-connects/m-p/1448119#M8759</guid>
      <dc:creator>mindchasers</dc:creator>
      <dc:date>2022-04-24T04:19:14Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A-FRWY system hangs when CodeWarrior connects</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-FRWY-system-hangs-when-CodeWarrior-connects/m-p/1448274#M8760</link>
      <description>&lt;P&gt;Do you want to use CodeWarrior to connect to the target board to do Linux Kernel debugging?&lt;/P&gt;
&lt;P&gt;If yes, please refer to CodeWarrior configuration in section 3 in this document.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-boot-and-Linux-Kernel-and/ta-p/1114872" target="_blank"&gt;https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-boot-and-Linux-Kernel-and/ta-p/1114872&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Apr 2022 05:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/LS1046A-FRWY-system-hangs-when-CodeWarrior-connects/m-p/1448274#M8760</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-04-25T05:27:07Z</dc:date>
    </item>
  </channel>
</rss>