<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Example MPC5674F eQADC+eDMA Continuous_Scan CW210 end at void EXCEP_DefaultExceptionHandler(void in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1395682#M8708</link>
    <description>&lt;P&gt;I am trying to do digital signal processing on one channel at says 100 200 kilo samples per seconds. Is it possible ?&lt;/P&gt;</description>
    <pubDate>Thu, 06 Jan 2022 14:45:24 GMT</pubDate>
    <dc:creator>pier-luc_rosa</dc:creator>
    <dc:date>2022-01-06T14:45:24Z</dc:date>
    <item>
      <title>Example MPC5674F eQADC+eDMA Continuous_Scan CW210 end at void EXCEP_DefaultExceptionHandler(void)</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1395054#M8705</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I am unable to run the following example.. using code warrior 10.7, but others example where working just fine..&lt;/P&gt;&lt;P&gt;What I did is create a new Project using a MPC5674F, copy *.c to source, *.h to Project_Headers&lt;/P&gt;&lt;P&gt;Then I deleted in source folder:&lt;/P&gt;&lt;P&gt;-__ppc_eabi_init.c&lt;/P&gt;&lt;P&gt;-MPC55xx_init.c&lt;/P&gt;&lt;P&gt;-MPC55xx_init_debug.c&lt;/P&gt;&lt;P&gt;-MPC5674F_MVxA264_HWInit.c&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 20:51:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1395054#M8705</guid>
      <dc:creator>pier-luc_rosa</dc:creator>
      <dc:date>2022-01-05T20:51:58Z</dc:date>
    </item>
    <item>
      <title>Re: Example MPC5674F eQADC+eDMA Continuous_Scan CW210 end at void EXCEP_DefaultExceptionHandler(void</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1395645#M8706</link>
      <description>&lt;P&gt;Hi, which moment it goes into exception? From the very beginning or somewhere from main routine?&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 13:57:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1395645#M8706</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-01-06T13:57:32Z</dc:date>
    </item>
    <item>
      <title>Re: Example MPC5674F eQADC+eDMA Continuous_Scan CW210 end at void EXCEP_DefaultExceptionHandler(void</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1395681#M8707</link>
      <description>&lt;P&gt;It is now working, not sure what was wrong with it (I believe connecting both potentiometer fixed the issue..) However, I added a pin toggle in the&amp;nbsp;eQADCA_FIFO0_EOQ_INT_handler and no matters what I do, when changing adc prescaler, it stay at 23Hz.. How can I increase the adc speed ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 14:41:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1395681#M8707</guid>
      <dc:creator>pier-luc_rosa</dc:creator>
      <dc:date>2022-01-06T14:41:34Z</dc:date>
    </item>
    <item>
      <title>Re: Example MPC5674F eQADC+eDMA Continuous_Scan CW210 end at void EXCEP_DefaultExceptionHandler(void</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1395682#M8708</link>
      <description>&lt;P&gt;I am trying to do digital signal processing on one channel at says 100 200 kilo samples per seconds. Is it possible ?&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 14:45:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1395682#M8708</guid>
      <dc:creator>pier-luc_rosa</dc:creator>
      <dc:date>2022-01-06T14:45:24Z</dc:date>
    </item>
    <item>
      <title>Re: Example MPC5674F eQADC+eDMA Continuous_Scan CW210 end at void EXCEP_DefaultExceptionHandler(void</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1395685#M8709</link>
      <description>&lt;P&gt;please see the comment above thanks&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 14:47:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1395685#M8709</guid>
      <dc:creator>pier-luc_rosa</dc:creator>
      <dc:date>2022-01-06T14:47:18Z</dc:date>
    </item>
    <item>
      <title>Re: Example MPC5674F eQADC+eDMA Continuous_Scan CW210 end at void EXCEP_DefaultExceptionHandler(void</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1396152#M8711</link>
      <description>&lt;P&gt;Just figured it out... The interrupt is taking too long to execute... The fix is to disable serial port printing&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jan 2022 12:39:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Example-MPC5674F-eQADC-eDMA-Continuous-Scan-CW210-end-at-void/m-p/1396152#M8711</guid>
      <dc:creator>pier-luc_rosa</dc:creator>
      <dc:date>2022-01-07T12:39:23Z</dc:date>
    </item>
  </channel>
</rss>