<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Code Warrior USB Tap &amp;quot;Device Protection Error&amp;quot; for IN28F640J3 in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-Warrior-USB-Tap-quot-Device-Protection-Error-quot-for/m-p/1388012#M8693</link>
    <description>&lt;P&gt;1. In PA Flash Programmer Task panel, target RAM&amp;nbsp; configuration, please specify the size of the RAM as 0x80000.&lt;/P&gt;&lt;P&gt;2. Please use initialization file&amp;nbsp;8548CDS_init_sram.tcl to avoid to configure DDR memory.&lt;/P&gt;&lt;P&gt;3. In CodeWarrior initialization file, please modify "configure Local Bus memory controller" section (BR0, OR0) according to your NOR flash. Please refer to MPC8548 reference manual for detailed description about register BR0 and OR0.&lt;/P&gt;</description>
    <pubDate>Thu, 16 Dec 2021 09:20:54 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2021-12-16T09:20:54Z</dc:date>
    <item>
      <title>Code Warrior USB Tap "Device Protection Error" for IN28F640J3</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-Warrior-USB-Tap-quot-Device-Protection-Error-quot-for/m-p/1387011#M8690</link>
      <description>&lt;P&gt;Hi everyone;&lt;/P&gt;&lt;P&gt;We've custom board with MCP8548 &amp;amp;&amp;nbsp;&lt;STRONG&gt;JS28F640J3F75A &lt;/STRONG&gt;NOR flash. We're using another debug probe to download binaries but we wanted to use Code Warrior USB Tap.&lt;/P&gt;&lt;P&gt;We configüred flash programmer&amp;nbsp;IN28F640J3 as NOR Flash but in some sectors we're getting "Device Protection Error" from CodeWarrior&lt;/P&gt;&lt;P&gt;Error seems like this:&lt;/P&gt;&lt;P&gt;* 0x00000 ~ 0x1FFFF --&amp;gt; Download &amp;amp; verify OK&lt;/P&gt;&lt;P&gt;* 0x20000 ~ 0x3FFFF --&amp;gt; Protection Error&lt;/P&gt;&lt;P&gt;* 0x40000 ~ 0x5FFFF --&amp;gt; Download &amp;amp; verify OK&lt;/P&gt;&lt;P&gt;* 0x60000 ~ 0x7FFFF --&amp;gt; Protection Error&lt;/P&gt;&lt;P&gt;So basically it seems one sector Ok, other sector Protection Error.&lt;/P&gt;&lt;P&gt;I'm also sending our debugger log as attachment&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp; &amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 07:06:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-Warrior-USB-Tap-quot-Device-Protection-Error-quot-for/m-p/1387011#M8690</guid>
      <dc:creator>mehmetalinbay</dc:creator>
      <dc:date>2021-12-15T07:06:35Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior USB Tap "Device Protection Error" for IN28F640J3</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-Warrior-USB-Tap-quot-Device-Protection-Error-quot-for/m-p/1388012#M8693</link>
      <description>&lt;P&gt;1. In PA Flash Programmer Task panel, target RAM&amp;nbsp; configuration, please specify the size of the RAM as 0x80000.&lt;/P&gt;&lt;P&gt;2. Please use initialization file&amp;nbsp;8548CDS_init_sram.tcl to avoid to configure DDR memory.&lt;/P&gt;&lt;P&gt;3. In CodeWarrior initialization file, please modify "configure Local Bus memory controller" section (BR0, OR0) according to your NOR flash. Please refer to MPC8548 reference manual for detailed description about register BR0 and OR0.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Dec 2021 09:20:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Code-Warrior-USB-Tap-quot-Device-Protection-Error-quot-for/m-p/1388012#M8693</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-12-16T09:20:54Z</dc:date>
    </item>
  </channel>
</rss>