<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: &amp;quot;CPE_TRACE_MSG_DMA_CFGERR, 0&amp;quot; error for DMA in CodeWarrior Development Tools</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-CPE-TRACE-MSG-DMA-CFGERR-0-quot-error-for-DMA/m-p/1336861#M8624</link>
    <description>&lt;P&gt;Hi, Yipingwang,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;Actually we just resolved the issue. The problem is that the AXI address (destination address) in our DMA statement is not 128-bit aligned, which is required in the document "VSPA-16SP ISA-v3.0 Instruction Set Manual for LA1224". After we change the address to 128-bit aligned address, we don't see the problem any more.&lt;/P&gt;</description>
    <pubDate>Wed, 08 Sep 2021 12:37:03 GMT</pubDate>
    <dc:creator>xuedongyang</dc:creator>
    <dc:date>2021-09-08T12:37:03Z</dc:date>
    <item>
      <title>"CPE_TRACE_MSG_DMA_CFGERR, 0" error for DMA</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-CPE-TRACE-MSG-DMA-CFGERR-0-quot-error-for-DMA/m-p/1334834#M8618</link>
      <description>&lt;P&gt;I am trying to DMA some data to HRAM for offline analysis in LA1224/LA2160 5G system. However, it kept saying DMA configuration error for this channel.&lt;/P&gt;&lt;P&gt;I checked the channel number, which is not used by anywhere else. Also I checked the HRAM address, which looks good. The DMA length is only 68 bytes. I am not sure what else could be wrong.&lt;/P&gt;&lt;P&gt;Anyone has any suggestion what else I should check. It is very annoying problem that is blocking our debugging activity.&lt;/P&gt;&lt;P&gt;Attached is the DMA statement I am using. Is there anything wrong in the statement? At least, I can compile and run.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Sep 2021 11:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-CPE-TRACE-MSG-DMA-CFGERR-0-quot-error-for-DMA/m-p/1334834#M8618</guid>
      <dc:creator>xuedongyang</dc:creator>
      <dc:date>2021-09-03T11:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: "CPE_TRACE_MSG_DMA_CFGERR, 0" error for DMA</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-CPE-TRACE-MSG-DMA-CFGERR-0-quot-error-for-DMA/m-p/1336633#M8623</link>
      <description>&lt;P&gt;Please give more information, what code is this? is this part of our LSDK? , which revision are we talking about, etc.?&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 07:29:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-CPE-TRACE-MSG-DMA-CFGERR-0-quot-error-for-DMA/m-p/1336633#M8623</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-09-08T07:29:12Z</dc:date>
    </item>
    <item>
      <title>Re: "CPE_TRACE_MSG_DMA_CFGERR, 0" error for DMA</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-CPE-TRACE-MSG-DMA-CFGERR-0-quot-error-for-DMA/m-p/1336861#M8624</link>
      <description>&lt;P&gt;Hi, Yipingwang,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;Actually we just resolved the issue. The problem is that the AXI address (destination address) in our DMA statement is not 128-bit aligned, which is required in the document "VSPA-16SP ISA-v3.0 Instruction Set Manual for LA1224". After we change the address to 128-bit aligned address, we don't see the problem any more.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 12:37:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/quot-CPE-TRACE-MSG-DMA-CFGERR-0-quot-error-for-DMA/m-p/1336861#M8624</guid>
      <dc:creator>xuedongyang</dc:creator>
      <dc:date>2021-09-08T12:37:03Z</dc:date>
    </item>
  </channel>
</rss>