<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: T1040d4 custom board without CPLD, JTAG programming issue</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/m-p/1252738#M8537</link>
    <description>&lt;P&gt;Please check whether your JTAG interface hardware design is similar as the following&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="yipingwang_0-1616749172774.png" style="width: 500px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/140740i21E90291A66A95B5/image-dimensions/500x613?v=v2" width="500" height="613" role="button" title="yipingwang_0-1616749172774.png" alt="yipingwang_0-1616749172774.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If the test fails to measure the length of the instruction register, then an error, Error measuring IR length, is thrown.&lt;BR /&gt;The error might be due to one or more of the following reasons:&lt;BR /&gt;• TRST stuck low: This may hold the target JTAG logic in reset, preventing any shifts to occur.&lt;BR /&gt;• TMS disconnected or stuck: This may prevent the target from making any JTAG state changes.&lt;BR /&gt;• TCK disconnected or stuck: This may prevent any state changes or clocking of data.&lt;BR /&gt;• TDI disconnected or stuck: This may prevent the test pattern data from getting into the target.&lt;BR /&gt;• TDO disconnected or stuck: This may prevent the test pattern data from getting out of the target.&lt;BR /&gt;If the test fails, then it is possible that there is a physical connection problem with the JTAG pins, or the JTAG frequency is too high.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 26 Mar 2021 09:03:05 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2021-03-26T09:03:05Z</dc:date>
    <item>
      <title>T1040d4 custom board without CPLD, JTAG programming issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/m-p/1252322#M8536</link>
      <description>Hi I have custom board designed using T1040d4 qoriq powerpc. My bareboard powerpc is currently power on using onboard power sequencing without using any CPLD. Right now i have no serial interface to monitor and debug it as both T1040 UART interfaced are attached with some other hardware over custom board. #Issue# when attached via CW usb tap its Jtag unable to program and flash bootloader via code warrior it shows " IR scan measure error" also "core not responding " in jtag log console.</description>
      <pubDate>Thu, 25 Mar 2021 17:11:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/m-p/1252322#M8536</guid>
      <dc:creator>Wj_khi</dc:creator>
      <dc:date>2021-03-25T17:11:12Z</dc:date>
    </item>
    <item>
      <title>Re: T1040d4 custom board without CPLD, JTAG programming issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/m-p/1252738#M8537</link>
      <description>&lt;P&gt;Please check whether your JTAG interface hardware design is similar as the following&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="yipingwang_0-1616749172774.png" style="width: 500px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/140740i21E90291A66A95B5/image-dimensions/500x613?v=v2" width="500" height="613" role="button" title="yipingwang_0-1616749172774.png" alt="yipingwang_0-1616749172774.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If the test fails to measure the length of the instruction register, then an error, Error measuring IR length, is thrown.&lt;BR /&gt;The error might be due to one or more of the following reasons:&lt;BR /&gt;• TRST stuck low: This may hold the target JTAG logic in reset, preventing any shifts to occur.&lt;BR /&gt;• TMS disconnected or stuck: This may prevent the target from making any JTAG state changes.&lt;BR /&gt;• TCK disconnected or stuck: This may prevent any state changes or clocking of data.&lt;BR /&gt;• TDI disconnected or stuck: This may prevent the test pattern data from getting into the target.&lt;BR /&gt;• TDO disconnected or stuck: This may prevent the test pattern data from getting out of the target.&lt;BR /&gt;If the test fails, then it is possible that there is a physical connection problem with the JTAG pins, or the JTAG frequency is too high.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Mar 2021 09:03:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/m-p/1252738#M8537</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-03-26T09:03:05Z</dc:date>
    </item>
    <item>
      <title>Re: T1040d4 custom board without CPLD, JTAG programming issue</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/m-p/1252886#M8538</link>
      <description>&lt;P&gt;Thanks for reply. TDI and TMS signals are pulled up with 10k resisters. This difference&amp;nbsp; i observed in your shared jtag logic schematic and with my followed t1040d4rdb "COP Connector " schematic section. Is there any effect of it regarding my jtag issue.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Mar 2021 13:11:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/m-p/1252886#M8538</guid>
      <dc:creator>Wj_khi</dc:creator>
      <dc:date>2021-03-26T13:11:13Z</dc:date>
    </item>
  </channel>
</rss>