<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: Tracing a program that jumps into RAM</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Tracing-a-program-that-jumps-into-RAM/m-p/1220067#M8521</link>
    <description>&lt;P&gt;If anyone else has this problem, move to the disassembled code window, scroll to the line you want, and click on it.&amp;nbsp; Same for the end of trace selection.&amp;nbsp; If that is documented anyplace, I didn't find it.&amp;nbsp; I just clicked on everything.&lt;/P&gt;</description>
    <pubDate>Mon, 25 Jan 2021 01:03:15 GMT</pubDate>
    <dc:creator>GaryOlmstead</dc:creator>
    <dc:date>2021-01-25T01:03:15Z</dc:date>
    <item>
      <title>Tracing a program that jumps into RAM</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Tracing-a-program-that-jumps-into-RAM/m-p/1173341#M8482</link>
      <description>&lt;P&gt;Hi --&lt;BR /&gt;I am using CW with a 9S08QE128.&amp;nbsp; The program is jumping into RAM and attempting to execute it.&amp;nbsp; I have the Profiling and Analysis Tools User Guide, and set up is pretty easy until it's time to enter "Address A" and "Address B".&amp;nbsp; Normally you click on the beginning and ending code you want to trace, but I want Address A to be address 0x0000 and B to be 0x1000, and the Profiling Guide doesn't have any way to do that.&lt;/P&gt;&lt;P&gt;To recap, on the Debug Configuration screen, I selected "Enable Trace and Profile", "Collect Program Trace",&amp;nbsp; "Automatically", "Collect Trace Until Trigger", Instruction Execute" and "Instruction Inside Range From Address A to Address B is Executed."&lt;/P&gt;&lt;P&gt;So how can I enter an address that I can't click on?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Gary Olmstead&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 20:57:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Tracing-a-program-that-jumps-into-RAM/m-p/1173341#M8482</guid>
      <dc:creator>GaryOlmstead</dc:creator>
      <dc:date>2020-10-26T20:57:21Z</dc:date>
    </item>
    <item>
      <title>Re: Tracing a program that jumps into RAM</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Tracing-a-program-that-jumps-into-RAM/m-p/1174687#M8488</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;I got a little bit lost. Are you using codewarrior? are you using P&amp;amp;E multilink? cyclone?&lt;/P&gt;
&lt;P&gt;Would be possible that you give a little bit more information about your problem&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a good day&lt;/P&gt;</description>
      <pubDate>Wed, 28 Oct 2020 18:26:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Tracing-a-program-that-jumps-into-RAM/m-p/1174687#M8488</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2020-10-28T18:26:49Z</dc:date>
    </item>
    <item>
      <title>Re: Tracing a program that jumps into RAM</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Tracing-a-program-that-jumps-into-RAM/m-p/1220067#M8521</link>
      <description>&lt;P&gt;If anyone else has this problem, move to the disassembled code window, scroll to the line you want, and click on it.&amp;nbsp; Same for the end of trace selection.&amp;nbsp; If that is documented anyplace, I didn't find it.&amp;nbsp; I just clicked on everything.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 01:03:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Tracing-a-program-that-jumps-into-RAM/m-p/1220067#M8521</guid>
      <dc:creator>GaryOlmstead</dc:creator>
      <dc:date>2021-01-25T01:03:15Z</dc:date>
    </item>
  </channel>
</rss>