<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックProgram NTM88 with USBDM in CodeWarior</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Program-NTM88-with-USBDM-in-CodeWarior/m-p/1199086#M8502</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I tried to compile and run demo for NTM88 in CodeWarior v11.1 using USBDM v4.12 and I have connection problem. As stated in instructions I have also installed patch "com.freescale.mcu11_1.HCS08_NTM88_LIB.win.sp.v1.0.2.zip".&lt;/P&gt;&lt;P&gt;When I try to run program from CodeWarior, it stops at 76% and reports one of following errors:&lt;/P&gt;&lt;P&gt;-"Error launching New_configuration"&lt;/P&gt;&lt;P&gt;-"USBDM - Target connection failure ... Retry connection ... yes/no"&lt;/P&gt;&lt;P&gt;Diagnostics report is in attachment.&lt;/P&gt;&lt;P&gt;I also tried using "HCS08 Programming" application it detects chip as "FXTH87" and I could also compare demo hex with program on chip (Verify flash) which naturaly reports difference.&lt;/P&gt;&lt;P&gt;I also tried changing settings of USDM, but without success.&lt;/P&gt;&lt;P&gt;Regards, Ales&lt;/P&gt;</description>
    <pubDate>Mon, 14 Dec 2020 17:52:29 GMT</pubDate>
    <dc:creator>alesgabersek</dc:creator>
    <dc:date>2020-12-14T17:52:29Z</dc:date>
    <item>
      <title>Program NTM88 with USBDM in CodeWarior</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Program-NTM88-with-USBDM-in-CodeWarior/m-p/1199086#M8502</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I tried to compile and run demo for NTM88 in CodeWarior v11.1 using USBDM v4.12 and I have connection problem. As stated in instructions I have also installed patch "com.freescale.mcu11_1.HCS08_NTM88_LIB.win.sp.v1.0.2.zip".&lt;/P&gt;&lt;P&gt;When I try to run program from CodeWarior, it stops at 76% and reports one of following errors:&lt;/P&gt;&lt;P&gt;-"Error launching New_configuration"&lt;/P&gt;&lt;P&gt;-"USBDM - Target connection failure ... Retry connection ... yes/no"&lt;/P&gt;&lt;P&gt;Diagnostics report is in attachment.&lt;/P&gt;&lt;P&gt;I also tried using "HCS08 Programming" application it detects chip as "FXTH87" and I could also compare demo hex with program on chip (Verify flash) which naturaly reports difference.&lt;/P&gt;&lt;P&gt;I also tried changing settings of USDM, but without success.&lt;/P&gt;&lt;P&gt;Regards, Ales&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 17:52:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Program-NTM88-with-USBDM-in-CodeWarior/m-p/1199086#M8502</guid>
      <dc:creator>alesgabersek</dc:creator>
      <dc:date>2020-12-14T17:52:29Z</dc:date>
    </item>
    <item>
      <title>Re: Program NTM88 with USBDM in CodeWarior</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Program-NTM88-with-USBDM-in-CodeWarior/m-p/1199652#M8503</link>
      <description>&lt;P&gt;Hello Ales,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We are not using USBDM so I cannot give feedback on it.&lt;/P&gt;
&lt;P&gt;We recommend using the P&amp;amp;E Micro USB Multilink Universal:&lt;/P&gt;
&lt;P&gt;&lt;A href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/mac57dxxx/universal-multilink-development-interface:UMultilink" target="_blank"&gt;http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/mac57dxxx/universal-multilink-development-interface:UMultilink&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 12:35:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Program-NTM88-with-USBDM-in-CodeWarior/m-p/1199652#M8503</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2020-12-15T12:35:05Z</dc:date>
    </item>
    <item>
      <title>Re: Program NTM88 with USBDM in CodeWarior</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Program-NTM88-with-USBDM-in-CodeWarior/m-p/1538224#M8881</link>
      <description>&lt;P&gt;have you found the solotion, i meet the same problem&lt;/P&gt;</description>
      <pubDate>Mon, 17 Oct 2022 03:39:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Program-NTM88-with-USBDM-in-CodeWarior/m-p/1538224#M8881</guid>
      <dc:creator>nguyenhuy5997</dc:creator>
      <dc:date>2022-10-17T03:39:35Z</dc:date>
    </item>
  </channel>
</rss>