<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior Development ToolsのトピックRe: Use codewarrior and PEMICRO to burn program for S08DZ60</title>
    <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Use-codewarrior-and-PEMICRO-to-burn-program-for-S08DZ60/m-p/1155089#M8451</link>
    <description>&lt;P&gt;Codewarrior 6.3 is not recommended to use with windows 7, you can have problems with the USB drivers&lt;/P&gt;
&lt;P&gt;Would be possible that you test it on code warrior 11?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 17 Sep 2020 23:00:01 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2020-09-17T23:00:01Z</dc:date>
    <item>
      <title>Use codewarrior and PEMICRO to burn program for S08DZ60</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Use-codewarrior-and-PEMICRO-to-burn-program-for-S08DZ60/m-p/1153232#M8447</link>
      <description>&lt;P&gt;Hi, I am using codewarrior V6.3 on a 32-bit windows 7 computer to program the S08DZ60 chip. The blue PEMICRO Multilink Universal is used, the version is Rev.D. But the following error occurs:&lt;BR /&gt;Loading Target ...&lt;BR /&gt;Windows NT detected.&lt;BR /&gt;P&amp;amp;E Interface detected-Flash Version 1..4&lt;BR /&gt;Frequency change to ~178321hz.&lt;BR /&gt;Device is 9S08DZ60.&lt;BR /&gt;Mode is In-Circuit Debug.&lt;BR /&gt;IO registers loaded for MC9S08DZ60 from C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.3\prog\REG\MCU1027.REG&lt;BR /&gt;executing BDM_P&amp;amp;E_Multilink_CyclonePro.hwc&lt;/P&gt;&lt;P&gt;done BDM_P&amp;amp;E_Multilink_CyclonePro.hwc&lt;/P&gt;&lt;P&gt;Error: The debugger is currently not able to run&lt;BR /&gt;due to loss of contact with hardware.&lt;BR /&gt;No Link To Target&lt;BR /&gt;——————————————————————————————————&lt;BR /&gt;But in another green version of the writer named Rev.C, it can burn successfully. The information is as follows:&lt;BR /&gt;Loading Target ...&lt;BR /&gt;Windows NT detected.&lt;BR /&gt;P&amp;amp;E Interface detected-Flash Version 6.15&lt;BR /&gt;Frequency change to ~15805785hz.&lt;BR /&gt;Frequency change to ~18042452hz.&lt;BR /&gt;Frequency change to ~8874709hz.&lt;BR /&gt;Device is 9S08DZ60.&lt;BR /&gt;Mode is In-Circuit Debug.&lt;BR /&gt;IO registers loaded for MC9S08DZ60 from C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.3\prog\REG\MCU1027.REG&lt;BR /&gt;Startup command file does not exist.&lt;BR /&gt;executing BDM_P&amp;amp;E_Multilink_CyclonePro.hwc&lt;/P&gt;&lt;P&gt;done BDM_P&amp;amp;E_Multilink_CyclonePro.hwc&lt;/P&gt;&lt;P&gt;Preload command file does not exist.&lt;BR /&gt;Frequency change to ~7968750hz.&lt;BR /&gt;executing C:\Users\Administrator\Desktop\Project\bin\Project.xpr&lt;/P&gt;&lt;P&gt;!Data:1 &amp;lt;ADDXPR ONLY_ADD_IF_NEW "AD_Trans_Value"&lt;BR /&gt;Target Ready&lt;BR /&gt;done C:\Users\Administrator\Desktop\Project\bin\Project.xpr&lt;/P&gt;&lt;P&gt;executing C:\Users\Administrator\Desktop\Project\bin\Project.xpr&lt;/P&gt;&lt;P&gt;!Data:1 &amp;lt;ADDXPR ONLY_ADD_IF_NEW "AD_Trans_Value"&lt;BR /&gt;MCU Device Selection has been changed.&lt;BR /&gt;done C:\Users\Administrator\Desktop\Project\bin\Project.xpr&lt;/P&gt;&lt;P&gt;Postload command file does not exist.&lt;BR /&gt;Frequency change to ~17957746hz.&lt;BR /&gt;STARTED&lt;BR /&gt;RUNNING&lt;BR /&gt;——————————————————————————————————&lt;BR /&gt;What may cause the Rev.D programmer to not work normally? It may be&lt;BR /&gt;Is the reason for "P&amp;amp;E Interface detected-Flash Version 6.15"&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 05:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Use-codewarrior-and-PEMICRO-to-burn-program-for-S08DZ60/m-p/1153232#M8447</guid>
      <dc:creator>964884547</dc:creator>
      <dc:date>2020-09-15T05:50:09Z</dc:date>
    </item>
    <item>
      <title>Re: Use codewarrior and PEMICRO to burn program for S08DZ60</title>
      <link>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Use-codewarrior-and-PEMICRO-to-burn-program-for-S08DZ60/m-p/1155089#M8451</link>
      <description>&lt;P&gt;Codewarrior 6.3 is not recommended to use with windows 7, you can have problems with the USB drivers&lt;/P&gt;
&lt;P&gt;Would be possible that you test it on code warrior 11?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Sep 2020 23:00:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-Development-Tools/Use-codewarrior-and-PEMICRO-to-burn-program-for-S08DZ60/m-p/1155089#M8451</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2020-09-17T23:00:01Z</dc:date>
    </item>
  </channel>
</rss>